2021-06-08 6:24 AM
I am working on a Nucleo-h745zi-q controller. I want to connect the stm32h7 board with Microsoft azure. I installed the package on stm32ide x-cube-azrtos-h7. But I did not know how I can connect to azure. What is the procedure for using this Rtos connectivity?
2021-06-08 8:30 AM
Hello @Kk and welcome to the Community :)
I added the right topics to your question in order to increase its chance to be reviewed by our experts, and I would also suggest you adding more details to your post in order to help you.
Maybe these links are useful for you:
Thanks
Imen
2021-06-08 1:04 PM
@Kk sorry but what is question / issue here ? Please be a little be more explicit if expecting some help ...
2021-06-09 12:18 AM
I am working on stm32h745zit6 controller. I want to connect the stm32h7 board with microsoft azure. I installed the package on stm32ide x-cube-azrtos-h7.But i did not know how i can connect to cloud azure. Means i have to do login to microsoft azure? What is the procedure for accessing the microsoft azure. Can you help me?
2021-06-09 4:38 AM
Hello,
The x-cube-azrtos-h7 package provides Azure RTOS support and NetX Duo network stack support on STM32H7. There is no specific support for Azure Cloud in this package. As you have Azure RTOS and network support on STM32H7 I guess you can just use Microsoft's examples and support for Azure IoT Cloud on their web site and github.
2021-06-09 4:43 AM
if you are using stm32h745zit6 , I don't see it in x-cube-azrtos-h7 package. So what kind of board are you using ? what network interface does it have ? ethernet ?
To be able to connect to Azure Cloud you need Azure RTOS and TCP/IP stack (NetX). If the network interface is not the same as the one supported in x-cube-AZRTOS-h7 you will have to implement in NetX Duo the network driver for it.
2021-06-09 4:46 AM
for MS Azure Cloud SDKs see https://github.com/Azure/azure-iot-sdks , especially Azure IoT SDK for embedded C
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.