STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7 Ethernet Destination MAC address

Hi Guys,I'm trying to do basic communication via Ethernet on a Nucleo H723 board. I would just like to send and receive a few Layer 2 frames. I'm going through the reference manual and the ETH HAL files to learn how the ethernet peripheral works. Wha...

USART BOOTLOADER launched from user application & flash has readout protection set, how can USART BOOTLOADER load new code to flash?

It seems unprotected flash can be programmed and then protected using user application launched native STM32 USART BOOTLOADER, but protected flash can only be cleared, but not reprogrammed without also having access to the boot pin configuration. (A...

PMoor.1 by Associate II
  • 2239 Views
  • 4 replies
  • 0 kudos

Resolved! Problem with USBPD

Hi,i am trying to use USBPD for my project. We are using the STM32G474RET in combination with the TCPP01-M12. In our application the STM32G4 should work as sink.I built a project for USBPD (with FreeRTOS), but the USBPD functions were just not call...

FIser.1 by Associate
  • 2047 Views
  • 1 replies
  • 1 kudos

How to set? fatfs runs at 50MHz?

I set sdmmc and fatfs at 50MHz.But under code error.res = f_mkfs(USERPath, FM_ANY, 0, workBuffer, sizeof(workBuffer)); if (res != FR_OK) { Error_Handler(); }sdmmc clock set 20MHz it is ok.Why sdmmc dosen't run at 50MHz?cubemx version : 6.2.0cubeide v...

JLee.21 by Associate II
  • 1583 Views
  • 2 replies
  • 0 kudos

STM32F429 CAN bus and USB VCP

Hi everyone, I have 32F429IDISCOVERY and I want to make some ''CAN to USB converter'', but when i choose CAN1 or CAN2 and USB device with Virtual COM port, device not identified in windows 10 with error 43 (A request for the USB device descriptor fai...

PAnde.2 by Associate
  • 1152 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.