STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB device whitout VBUS

Hello, I have a problem with USB device and VBUS, I have tried on several posts but I have not found the solution.I try to explain, I use STM32H743, USB_OTG_HS, USB_DEVICE, COMUNICATION DEVICE CLASS and the problem is precisely VBUS which enters on p...

mBosc.11 by Associate II
  • 3291 Views
  • 3 replies
  • 0 kudos

STM32L4 SD CARD FATFS Example not working

Hello,I have a system based on STM32L452 with SDCARD. I can read and write in the SD card using the HAL functions but when I try to integrate the FATFS file system I have issues with DMA when trying to read/write to the SDA card (interrupts never arr...

I am using STM32nucleof446re board and using freeRTOS as third party.I made two simple tasks which used printf statement that "task1/2 is running "​.But when I want to debugge mode and started tracing then I am unable to see anything on ITM console.

I am using STM32nucleof446re board and using freeRTOS as third party.I made two simple tasks which used printf statement that "task1/2 is running ".But when I want to debugge mode and started tracing then I am unable to see anything on ITM console.I ...

SGupt.10 by Associate
  • 1429 Views
  • 1 replies
  • 0 kudos

Resolved! HAL/LL documentation?

Hello all,Is there a reference doc about the HAL/LL for ST's 32F439 ARM MCU?  I want to know the function structure and just want to know how it works and to have control over how I set up my devices.thanks George 

gdori.1 by Associate II
  • 1174 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.