2021-06-08 4:48 AM
It is working firmware STM32H7-DISCO with freeRTOS using internal flash. Almost full my binary. I planned to develop my firmware internal flash to SRAM. I modified .ld file and able to boot SRAM. Please check the below changes.
/* Memories definition */
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
RAM_D1 (xrw) : ORIGIN = 0x24040000, LENGTH = 256K
RAM_D2 (xrw) : ORIGIN = 0x30000000, LENGTH = 288K
RAM_D3 (xrw) : ORIGIN = 0x38000000, LENGTH = 64K
FLASH (rx) : ORIGIN = 0x24000000, LENGTH = 256K //change interflash to ram 0x08000000
}
But it is hanging in kernelstart() -> prvPortStartFirstTask() funtion (0xE000ED08 have 0x8000000 flash address) . I used STMCUBEID generate code. Even i tried external flash using QSPI . It is hanging same function.
It is working fine without FreeRTOS for external flash and internal ram.
Do i need to change any other setting for change FLASH?
2021-06-17 5:41 AM
Hello,
Have you tried the STM32CubeH7 firmware examples ?
The firmware packages provide several applications to demonstrate how to boot from internal Flash memory and how to configure the external memories and jump to user application (located on the external memory).
Also, I advise you to have a look to AN5188 Maybe it can help you.
Imen
2021-06-28 10:07 PM
Hi ,
It resolved the issue . I modified loader file and flash load in below header file.
Drivers\CMSIS\Device\ST\STM32H7xx\Include\stm32h750xx.h
#define FLASH_BASE D1_AXISRAM_BASE //0x24000000
Core/src/system_stm32h7xx.c
SCB->VTOR = FLASH_BASE | VECT_TAB_OFFSET; /* Vector Table Relocation in Internal FLASH */
Thanks
Rajesh Kannan
2021-06-29 9:39 AM
In Keil
extern void *__Vectors;
SCB->VTOR = (uint32_t)&__Vectors; /* Vector Table Relocation */
In GNU
extern void *g_pfnVectors;
SCB->VTOR = (uint32_t)&g_pfnVectors; /* Vector Table Relocation */
Saves hours of time wasting, and makes the linker/compiler do the jobs they were assigned to do.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.