STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problem Sending MQTT messages using FreeRTOS

Hello,I have an FreeRTOS task that sends 4 MQTT messages (using LwIP MQTT) every 10 seconds:void HomeAssistantConfigTask(void *argument) { /* USER CODE BEGIN HomeAssistantConfigTask */ /* Infinite loop */ for(;;) {   SendAvailabilityMessa...

STM32F723 I2C bootloader : No-Stretch Erase command leads to long clock stretching anyway. How to deal with it?

Several questions: The I2C bootloader answers version 1.2 which is not documented in AN4221 even though it was recently updated in June 2021. Is it planned to publish this information soon?I am sending a "No-stretch Erase" command via the following o...

YSion.1 by Associate
  • 1605 Views
  • 2 replies
  • 2 kudos

Resolved! Multiple I²C slaves with FREERTOS

Hi,I am using 2 slaves on the I²C bus : touchscreen and FRAM.I am calling BSP_TS_GetState in the sampleTouch function.bool STM32TouchController::sampleTouch(int32_t& x, int32_t& y) { bool ret = false;   if (!i2cUsed) { i2cUsed |= 2; TS_StateTy...

MMerc.1 by Senior
  • 2237 Views
  • 2 replies
  • 0 kudos

STN32H747 Dual Core - only reset 1 core

I can perform a software system reset but what I want to do is have the M7 reset the M4 cpu - is there a way?I have always written my own bootloader so the product can have firmware upgraded in the field.With the Dual Core - the M7 will be updating t...

Joe.H by Senior
  • 2393 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F7 ethernet PTP PPS to timer 2

Hello,I just got lwIP with PTPd on 2 Nucleo-144 with STM32F767ZI working.Thanks to all the open source people out there!PPS output is also working, I use these signals to check sync quality on a scope.PPS from ETH goes to TIM2 via ITR1 input to TRGO ...

LCE by Principal II
  • 8866 Views
  • 13 replies
  • 2 kudos

STM32F407VGT7 I use system memory boot mode by USART1 (PA10, PA9). i have to use external pull-up/pull-down resistors to USART3 (PB10 / PB11, PC10 / PC11), CAN2 (PB5), USB (PA11, PA12)?

STM32F407VGT7 I use system memory boot mode by USART1 (PA10, PA9). i have to use external pull-up/pull-down resistors to USART3 (PB10 / PB11, PC10 / PC11), CAN2 (PB5), USB (PA11, PA12)?PA10, PA9 connect to external pull-up resistors 7.5Kohms.If don't...

VDil.1 by Associate
  • 1321 Views
  • 1 replies
  • 0 kudos

When I plug in 64 and 128 gb usb, it says the library is constantly connected and disconnceted. But 16gb usb works clearly.

Hello,I use USB MSC modules codes which provided by ST ( HAL Library USB )Actually I can use correctly my application with 16GB ,8GB ,4GB USB.But When I plug in 64GB USB or 128GB, it is not working.it is periodically transmit "USB Device disconnecte...

cvarl.1 by Associate
  • 1489 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.