2021-10-27 10:58 AM
Hi,
I'm using X-CUBE-AWS 2.2.0 with a B-L4S5I-IOT01A dev board. While trying to provision and save the keys, the erase function HAL_Erase_Data_Zone() is returning the error STSAFEA_KEY_BLOCKED. I have made sure that DBANK is 0. I enabled PRINTF_ON and here is the output:
Launching STSAFE-A pairing
Check if Pairing Host keys available
use default keys and meanwhile set buf = NULL
Check_host_keys STSAFEA_OK
Set access condition to host for Zone 2 & 3 & 4
Pairing OK
Size of data's to be send exceed max size of STSAFE-Axx buffer
We have to split data's in blocks
ERROR: StatusCode StSafeA_Update=0xb
Size of data to copy 9
ERROR: StatusCode StSafeA_Update=0xb
Size of data to copy 9
ERROR: StatusCode UpdateZone=0xb
ERROR: StatusCode =0xb
Erase data NOK, to understand source of the error please enable log
using #define PRINTF_ON, End of Provisioning !!!!
Any idea what might be causing this error? Is there another option byte I have to change?
Thanks in advance.
Hank
2021-12-03 2:42 AM
Hi Hank,
Actually, you have blocked the Pairing keys of your STSAFE-A due to too many invalid C-MAC operation in row (more than 50).
You can no longer use the Host Keys on this STSAFE-A, you need to change it.
Did you make modification in the B-L4S5I-IOT01A STSAFE Provisioning ?
For your next trial with a new STSAFE-A, you can run the STSAFE Provisioning a first time without issue as long as the pairing is not done on the STSAFE-A.
If you want to reload the STSAFE Provisioning after a mass erase of the flash (due to RDP regression for instance) then you need to set the #define FORCE_PAIRING in order to make sure that the flash has been updated.
Alternative solution is to change the #define USE_PRE_LOADED_HOST_KEYS to 0 in the stsafea_interface_conf.h
Best Regards,
Benjamin BARATTE
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.