2021-11-24 3:34 AM
2021-11-24 10:55 PM
@JAgni.1 Check the USB Port Pins are same and Clock Settings . In schematics check the MIC (Analog or Digital). If you have same target board working fine, Check once more .
If target board share the error then the it could be the cable or debugging connection issue
2021-11-25 4:22 AM
@Snara.2 Thank you for your quick reply. I have checked USB Port pins and clock settings. That error message is gone now, there was issue with USB cable. But still STM32F446RE not getting detected as USB Mic. I am using only mic node of X-CUBE package. I have ported Application/User files to my own project keeping Board support package,drivers as it is(hardware). Do I need to do any setting for USB enumeration? I have been stuck at this point for many days. I appreciate your help.
2021-12-06 4:19 AM
Hello,
I have resolved that USB enumeration issue. But using X-CUBE-USB-AUDIO package, I am not able to record any voice. Is there any utility that needs to be use to make this package work properly? Please help me. Thank you in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.