STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! is STM32F7 has DFSR register?

Hi!I try to understand debug information after hard fault. RTOS dump DFSR register (and some other) after fault to UART. This register is not present in PM0253 programming manual, but there is definition in source code (core_cm7.h address is 0xE000ED...

Aleks by Associate III
  • 1541 Views
  • 3 replies
  • 2 kudos

Resolved! Does the DMA Arbiter allow round robin preemption after each piece of data to keep multiple peripherals going at once or does the DMA controller completely block until an entire block of data has finished transmitting?

I am working with the STM32L4S9AII6 MCU on a project where I am being asked to replace an FPGA implementation with this CPU. We are maxing out all 14 DMA streams via SPIs, I2Cs, & UART. As you can imagine, I am working with some serious hard real-tim...

MFolk.1 by Senior
  • 1729 Views
  • 2 replies
  • 0 kudos

Resolved! Configure SDMMC2 for H743VIT6

Hi,1- How do I let CubeMX know the SD pin detect, I've set pin PC13 as card_detect, GPIO input, pull-up, but then what?2- Should I use the open source FATFS "https://elm-chan.org/fsw/ff/00index_e.html"? How?Thank you

ksale.1 by Senior II
  • 1908 Views
  • 4 replies
  • 0 kudos

RTOS multiple uart

Hello,there is some solution for sending data over multiple uarts with RTOS,because HAL_UART_Transmit,HAL_UART_Transmit_IT,HAL_UART_Transmit_DMA not send data in second uart. Still BUSY.Thank you in advantages

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.