cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a socket allocation problem with X-CUBE-CELLULAR V7.0 using Azure RTOS and the STM32L462RE discovery kit Cellular IOT board?

JVand.12
Associate II

In this loop the mqtt client is created, connected and as long as the mqtt server/broker is up, the client continues processing messages. But when the remote mqtt server/broker is manually shut down, and after the timeout expires, nxd_mqtt_client_connect is called repeatedly. For the first six iterations it acquires socket descriptors starting with the value of 0 and that increases to 5. There are only 6 sockets available in the Murata modem. After that the socket descriptor is not correct. The mqtt client cannot reconnect when the remote mqtt server/broker is again started.

*************************** Trace ****************

client disconnected from server

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 0 

LOG ERROR #7: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 1 

LOG ERROR #8: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 2 

LOG ERROR #9: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 3 

LOG ERROR #10: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 4 

LOG ERROR #11: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 5 

LOG ERROR #12: channel=1 / errorId=7 / gravity=2

com connect status 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

Modem state     : 5

IP address : 100.96.129.90

Trying to connect MQTT broker

MQTT client socket binding status 0 

com socket create success socket fd 4294967295 

MQTT client socket 1413697568 

MQTT tcp client socket connect status 86 

MQTT tcp client socket unbind status 0 

MQTT connect status 65541 

***************** Loop fragment ********

while (1) {

 switch (state) {

case 0:

/* Wait Link/Data is enabled before to do/send data on network. */

status = nx_ip_interface_status_check(p_IpInstance, 0U, NX_IP_LINK_ENABLED, &link_status,

 10000); /* 3); => MISRAC2012-Rule-7.2 */

if (status == (UINT)NX_SUCCESS)

{

state = 2;

}

case 1:

t4 = HAL_GetTick();

if ((t4-t3)>(1*10*1000)) {

t3 = HAL_GetTick();

state = 2;

}

break;

case 2:

(void)printf("App starting MQTT creation\n\r");

status = nxd_mqtt_client_create(&mqtt_client, "my_client",

CLIENT_ID_STRING, STRLEN(CLIENT_ID_STRING), p_IpInstance, p_AppPool,

(VOID*)mqtt_client_stack, sizeof(mqtt_client_stack),

MQTT_THREAD_PRIORTY, NX_NULL, 0);

if (status == NXD_MQTT_SUCCESS) {

nxd_mqtt_client_login_set(&mqtt_client,

MQTTNAME, STRLEN(MQTTNAME),

MQTTPASS, STRLEN(MQTTPASS));

/* Register the disconnect notification function. */

nxd_mqtt_client_disconnect_notify_set(&mqtt_client, my_disconnect_func);

/* Create an event flag for this demo. */

ev_status = tx_event_flags_create(&mqtt_app_flag, "my app event");

server_ip.nxd_ip_version = 4;

server_ip.nxd_ip_address.v4 = MQTT_SERVER_ADDRESS;

state = 3;

t5 = HAL_GetTick();

}

break;

case 3:

/* Start the connection to the server. */

(void)printf("Trying to connect MQTT broker\n\r");

nxd_mqtt_client_login_set(&mqtt_client,

MQTTNAME, STRLEN(MQTTNAME),

MQTTPASS, STRLEN(MQTTPASS));

status = nxd_mqtt_client_connect(&mqtt_client, &server_ip, NXD_MQTT_PORT,

MQTT_KEEP_ALIVE_TIMER, 0, 10000);//NX_WAIT_FOREVER

(void)printf("MQTT connect status %u \n\r", status);

if (status == NXD_MQTT_SUCCESS || status == NXD_MQTT_ALREADY_CONNECTED) {

/* Subscribe to the topic with QoS level 0. */

nxd_mqtt_client_subscribe(&mqtt_client, TOPIC_NAME2, STRLEN(TOPIC_NAME2),

QOS0);

/* Set the receive notify function. */

nxd_mqtt_client_receive_notify_set(&mqtt_client, my_notify_func);

state = 4;

break;

} else if (status == NXD_MQTT_CONNECTING) {

state = 3;

break;

}

else {

t6 = HAL_GetTick();

if ((t6-t5)>(1*15*1000)) {

nxd_mqtt_client_delete(&mqtt_client);

state = 2;

t5 = HAL_GetTick();

break;

}

}

*/

break;

case 4:

/* Publish a message with QoS Level 1. */

state = 6;

t2 = HAL_GetTick();

if ((t2-t1)>(1*30*1000)) {

t1 = HAL_GetTick();

(void)printf("MQTT publishing start \n\r");

status = nxd_mqtt_client_publish(&mqtt_client, TOPIC_NAME,

STRLEN(TOPIC_NAME), (CHAR*)MESSAGE_STRING,

STRLEN(MESSAGE_STRING), 0, QOS1, 10000);

(void)printf("MQTT publish status %u \n\r", status);

if (status == NXD_MQTT_SUCCESS) {

state = 6;

} else

{

state = 3;

t5 = HAL_GetTick();

}

}

tx_event_flags_get(&mqtt_app_flag, DEMO_ALL_EVENTS,

TX_OR_CLEAR, &events, 5000);

break;

case 5:

break;

case 6:

if(events & DEMO_MESSAGE_EVENT)

{

nxd_mqtt_client_message_get(&mqtt_client, topic_buffer,

sizeof(topic_buffer), &topic_length, message_buffer,

sizeof(message_buffer), &message_length);

topic_buffer[topic_length] = 0;

message_buffer[message_length] = 0;

printf("topic = %s, message = %s\n\r", topic_buffer, message_buffer);

}

state = 4;

break;

 }

 }

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.