cancel
Showing results for 
Search instead for 
Did you mean: 

HAL QSPI AUTOPOLLING SUPPORT 4LINES?

JCuna.1
Senior

I have read many samples in cube h7 github repository, and I have seen any hal autoplling example consulting status registers in 4 lines mode operation. It is supported? I am using STM32H750 with cube h7 1.10.0.

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4

What make/model memory device are you using?

S​eem to recall you using Bank 2

Show initialization code, paste as quoted text, not graphic. See </> icon.

PB2 CLK​

PC11 BK2 NCS

PE7 BK2​ D0

PE8

PE9

PE10 BK2 D3​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
JCuna.1
Senior
/* QUADSPI init function */
void MX_QUADSPI_Init(void)
{
 
  /* USER CODE BEGIN QUADSPI_Init 0 */
 
  /* USER CODE END QUADSPI_Init 0 */
 
  /* USER CODE BEGIN QUADSPI_Init 1 */
 
  /* USER CODE END QUADSPI_Init 1 */
  hqspi.Instance = QUADSPI;
  hqspi.Init.ClockPrescaler = 9;
  hqspi.Init.FifoThreshold = 1;
  hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
  hqspi.Init.FlashSize = 21;
  hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_1_CYCLE;
  hqspi.Init.ClockMode = QSPI_CLOCK_MODE_3;
  hqspi.Init.FlashID = QSPI_FLASH_ID_2;
  hqspi.Init.DualFlash = QSPI_DUALFLASH_DISABLE;
  if (HAL_QSPI_Init(&hqspi) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN QUADSPI_Init 2 */
 
  /* USER CODE END QUADSPI_Init 2 */
 
}
 
void HAL_QSPI_MspInit(QSPI_HandleTypeDef* qspiHandle)
{
 
  GPIO_InitTypeDef GPIO_InitStruct = {0};
  RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
  if(qspiHandle->Instance==QUADSPI)
  {
  /* USER CODE BEGIN QUADSPI_MspInit 0 */
 
  /* USER CODE END QUADSPI_MspInit 0 */
 
  /** Initializes the peripherals clock
  */
    PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_QSPI;
    PeriphClkInitStruct.QspiClockSelection = RCC_QSPICLKSOURCE_D1HCLK;
    if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
    {
      Error_Handler();
    }
 
    /* QUADSPI clock enable */
    __HAL_RCC_QSPI_CLK_ENABLE();
 
    __HAL_RCC_GPIOB_CLK_ENABLE();
    __HAL_RCC_GPIOE_CLK_ENABLE();
    __HAL_RCC_GPIOC_CLK_ENABLE();
    /**QUADSPI GPIO Configuration
    PB2     ------> QUADSPI_CLK
    PE7     ------> QUADSPI_BK2_IO0
    PE8     ------> QUADSPI_BK2_IO1
    PE9     ------> QUADSPI_BK2_IO2
    PE10     ------> QUADSPI_BK2_IO3
    PC11     ------> QUADSPI_BK2_NCS
    */
    GPIO_InitStruct.Pin = GPIO_PIN_2;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_PULLUP;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
    HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 
    GPIO_InitStruct.Pin = GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF10_QUADSPI;
    HAL_GPIO_Init(GPIOE, &GPIO_InitStruct);
 
    GPIO_InitStruct.Pin = GPIO_PIN_11;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
    GPIO_InitStruct.Alternate = GPIO_AF9_QUADSPI;
    HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
 
  /* USER CODE BEGIN QUADSPI_MspInit 1 */
 
  /* USER CODE END QUADSPI_MspInit 1 */
  }
}
 
void HAL_QSPI_MspDeInit(QSPI_HandleTypeDef* qspiHandle)
{
 
  if(qspiHandle->Instance==QUADSPI)
  {
  /* USER CODE BEGIN QUADSPI_MspDeInit 0 */
 
  /* USER CODE END QUADSPI_MspDeInit 0 */
    /* Peripheral clock disable */
    __HAL_RCC_QSPI_CLK_DISABLE();
 
    /**QUADSPI GPIO Configuration
    PB2     ------> QUADSPI_CLK
    PE7     ------> QUADSPI_BK2_IO0
    PE8     ------> QUADSPI_BK2_IO1
    PE9     ------> QUADSPI_BK2_IO2
    PE10     ------> QUADSPI_BK2_IO3
    PC11     ------> QUADSPI_BK2_NCS
    */
    HAL_GPIO_DeInit(GPIOB, GPIO_PIN_2);
 
    HAL_GPIO_DeInit(GPIOE, GPIO_PIN_7|GPIO_PIN_8|GPIO_PIN_9|GPIO_PIN_10);
 
    HAL_GPIO_DeInit(GPIOC, GPIO_PIN_11);
 
  /* USER CODE BEGIN QUADSPI_MspDeInit 1 */
 
  /* USER CODE END QUADSPI_MspDeInit 1 */
  }
}

 My code works for read or write operation (polling only wel bit). But for erase operation I need to poll wel and wip/busy bit. I am using W25Q32JVSSIM-TR.

Other L4 examples break the register read into a more normal interaction/loop

The auto-poll should work, not sure if there is any errata. You have the Y or V step of the H750 ? Doubt you have Z or X's

https://www.st.com/resource/en/errata_sheet/es0396-stm32h750xb-and-stm32h753xi-device-limitations-stmicroelectronics.pdf Nothing jumping out..

Does it really need you looking at both bits? BUSY is the thing you need to spin on

Try the Mode 0 clock mode. ie where it doesn't idle high

05h should work in 1-bit and 4-bit, mode? Make sure spimode is right, that QE is set, and Quad Mode is enabled (38h), won't be by default. It will exit QPI if FFh is clocked as a command

QE is in SR2, and SR1/SR2 need to be written as a pair

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Cross linking other thread to help find them later https://community.st.com/s/question/0D53W00001WJBQOSA5/qspi-strange-behavior-when-autopolling

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.