STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UM0391, Is There A 2nd Testament?

Workalot is working on a DfuFileMgr 'look a like' (wdfufm if you will). It is to be embedded within a PC application.A first run through of 'wdfufm' establishes UM0391, 15-Feb-2007, sec 2.1, page 4 (aka 1st testament) misleads. In particular with th...

Workalot by Associate III
  • 908 Views
  • 0 replies
  • 0 kudos

STM32U585 serial programming (Embedded Linux)

Hi,Is there a way to program STM32U585 MCU via USART1 peripheral using Embedded Linux processor? Except BOOT0 pin and RESET pin of U5 MCU what else need to be done to get into Serial Programming mode? Thanks in advance,Nenad

NGajic by Associate III
  • 2098 Views
  • 2 replies
  • 0 kudos

usb host fat32 does not work with freeRTOS

I have stm32f429discovery and i used stm32cubeMx to set up usb host with fast32. when I connect flash it works OK. but when I configure freeRTOS it didn't work. when i debug it, I found it go to "HardFault_Handle" loop. i increase heap and stack size...

Javad by Associate III
  • 4220 Views
  • 5 replies
  • 1 kudos

STM32 MW USB Host Library v3.4.0 release on GitHub

What is new in STM32 USB Host Library v3.4.0?*           Core driver :Fixes added to free RTOS resource during USB host DeInitCodeSpell and mcuAstlye fixesMultiple MisraC 2012 fixes*           All Classes :CodeSpell and mcuAstlye fixesMultiple MisraC...

STM32G0B1 USB PD NO UTILITY OS infinite loop.

When generating code with CubeMX for an USBPD sink application for the STM32G0B1 when no RTOS is used within the function USBPD_DPM_Run on line 340 till 363 it enters an inifinite do while loop. This happens in the usbpd_dpm_core.c file.It is undesir...

JBand.2 by Associate II
  • 1908 Views
  • 1 replies
  • 0 kudos

Unable to boot from bank2 with L073RZ

Hi,I have a simple application that I flashed to 0x0800 0000 and 0x0801 0000 using STM32CubeProgrammer. With BFB2 unchecked, the app runs correctly from bank1 but when I check BFB2 to boot from bank2 it looks like the board get stuck somewhere as the...

AlexS by Associate II
  • 2040 Views
  • 4 replies
  • 0 kudos

STM32F072R8 does not enter into DFU mode

Hello,I have custom board with STM32F072R8 and a USB interface to it. STM's USB is connected to USB of a x86 Board. STM as acting as USB device and x86 Board as USB host. When the board is powered up, I can see that STM is listed in the output of "ls...

ab_nurd by Associate II
  • 1496 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.