STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Application doesn't work when loaded through USB DFU

Hello,I am working on the USB DFU for a STM32H7A3ZGT6I have two projects one for the DFU and one with the application to be updated.My application works fine when I download it with the debugger.The DFU part manages to erase and program the new app t...

ABricout by Associate III
  • 2953 Views
  • 6 replies
  • 0 kudos

Auto detect STM32G0 Variations? Or pc_init, pc_unInit, pc_program_page, pc_erase_sector, pc_eraseAll, static base, begin stack, end stack, begin data, page size, page buffers address in mcu?

I am using PyOCD and CMSIS Pack Manager to connect and read from my MCU. However, to write I need to know the specific MCU name such STM32g071cbux. Is there a way to autodetect that variation between like STM32g071cbTx. or can I auto detect like my p...

LMora.5 by Associate
  • 2314 Views
  • 3 replies
  • 0 kudos

Resolved! STM32L071 - RTC ISR flags clearing

In the following HAL function, RTC ISR register is cleared by "Read/Modify/Write" instruction.Couldn't this cause eventual clearing of the ISR flags which may be raised by RTC periphery between "load" AND "store" ?If somebody can confirm that such si...

MPrud.1 by Associate
  • 2070 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.