STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! But it is normal to write single blocks continuously (cmd24), but the speed is a little slow. I use FatFs to write multiple blocks (cmd25) to SD card. I can only create a new TXT file, but there is no data in it.

But it is normal to write single blocks continuously (cmd24), but the speed is a little slow. I use FatFs to write multiple blocks (cmd25) to SD card. I can only create a new TXT file, but there is no data in it. And when writing multiple blocks, the...

0693W00000QMzyPQAT.png 0693W00000QMzsrQAD.png
Lep by Senior
  • 1832 Views
  • 2 replies
  • 0 kudos

undefined symbol ossemaphorecreate

Why the API for FreeRTOS middleware keeps changing every now and then? You barely start to wrap your head around an API, a new one gets released. I had to generate the initialization code from CubeMX, as it makes life much easier especially if you wa...

Zaher by Senior II
  • 3399 Views
  • 3 replies
  • 0 kudos

Resolved! LwIP on the CM4 core of a dual core STM32H7?

Has anyone been successful using CubeMX to create a CubeIDE bare metal project with Ethernet/LwIP running on the CM4 core of a dual-core STM32H7 processor?If so, I'd greatly appreciate any pointers or examples you can share.

WLear by Associate III
  • 2781 Views
  • 3 replies
  • 0 kudos

Is it guaranteed that the original pointer is passed from the interrupt handlers to the callbacks when using HAL?

I would like to implement a C++ wrapper around the STM32 HAL. I have a class called I2C_Handler, which manages the usual I2C HAL structs and functions. The only problem that I am having now are the callbacks, because the callbacks functions called by...

USBX-Host on NUCLEO-U575ZI

Is there any working example for this board (NUCLEO-U575ZI) where I can learn how to write files on a USB Hard Drive connected over the USB-Type C port using USBX and FILEX?On CubeIDE I found an example Ux_Host_MSC regarding STM32U575I-EV but cannot...

hi, i got a STEVAL-STWINKT1B i would like to run STM32CubeFunctionPack_DATALOG1_V1.3.0, am i able to display the data in real-time while it is writing into .dat file by USB ?

i have found this line in the python_SDK but there is no such function.# NOTE here you can queue sensor data (to process or display them)          # NOTE: e.g. -> self.hsd_info.queue_sensor_data([sensor_data])i

YTan.5 by Associate II
  • 839 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.