STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H750 + USB3300 | No signals on ULPI

Hi guys, i am at a complete loss; even with describing the problem.I have a 6-layer board with the USB3300 directly underneath the H750(100Pin LQFP), so traces are short and basically optimal. I use CubeMX to generate an example -> I use MCO2 as 24MH...

Albi G. by Senior
  • 9986 Views
  • 9 replies
  • 1 kudos

AzureRtos tickless mode support status?

Hello Dears, the last update from ST related to tickless mode for AzureRtos was back in January 2021, here, is there any new update on this? I'm asking specifically for the L4.It isn't obvious to have the option in CubeMx when the feature is not full...

Waelha by Associate II
  • 1188 Views
  • 1 replies
  • 0 kudos

Is there a good example for I2S on F0?

Greetings Everyone.I am trying to create a Firmaware based on F0 (library 1.11.3) to MASTER ONLY READING using the I2S protocol.I have an IC which sends a DATA READY and only waits for a clock pulses to shift-out the complete data (24-bit frame). The...

JSILV.2 by Senior
  • 2720 Views
  • 5 replies
  • 0 kudos

HAL_UARTEx_ReceiveToIdle_IT - meaning of idle ?

Dear ST/reader,I’m currently implementing a uart receive interrupt function for use with the STM32H743 specifically using HAL_UART_Receive_IT(). This is straightforward when the receive length (number of bytes to receive) is just 1 in which case it e...

TMA1of3 by Associate III
  • 11210 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.