STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

config MPU

Hi, I have started working with MPU and I can see from the examples the potential of this caracteristic. I am developing a safety app in which there are two parts in the program: Safety and no-safety application. Meanwhile the part of the ADC is safe...

OAgui.1 by Associate II
  • 1429 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F7 - USB High Speed User experience?

Hello,I have just "finished" the ethernet interface for a STM32F7, now we think about also using the USB high speed interface (yes, it needs an external high speed USB PHY), that would be for data streaming, as an alternative for using ethernet, as m...

LCE by Principal II
  • 3944 Views
  • 4 replies
  • 0 kudos

Resolved! STM32F7: small package, hi-speed ext. SRAM, please

Hello community,now that STM32F767 + lwIP / TCP is working well, I found that sometimes it takes too long for streaming that the other side gets the data (some other network traffic, or delayed ACKs, or whatever Windows does), and the STM32's interna...

LCE by Principal II
  • 3492 Views
  • 7 replies
  • 0 kudos

NUCLEO-H755ZI-Q deadlock

We have been testing a NUCLEO-H755ZI-Q by creating example projects using STM32CubeMx, which work fine. However, given the microcontroller is dual core, we felt the need to investigate the different boot options it offers in order to make it compatib...

0693W00000UFMGBQA5.png 0693W00000UFMJZQA5.png 0693W00000UFMJjQAP.png 0693W00000UFMJoQAP.png
RTira.1 by Associate II
  • 1754 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with USB in virtual port com

Hi Everybody,I've got a few problems with my USB. I have configured the USB port of my STM32L476 in communication device class (virtual port com).I can send and receive data on my terminal.What I'm doing is the following : sprintf(buf,BYTE_TO_BINARY_...

fab04 by Senior
  • 2017 Views
  • 3 replies
  • 0 kudos

Resolved! (stm32h732) usb device, How can i transfer data with desired speed 1 Mbytes / sec in Full speed mode?

I need to transmit data over usb with minimum 1 Mb/s, I configured my mcu (stm32h732zg) as an audio device to get a large packet transfer.the function that transfer the data USBD_AUDIO_DataIn is empty. and USBD_CtlSendData i'm using cause the usb des...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.