STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lwip tcp server problem solution please

I made this sauce to implement lwip tcp serverIf you try to remove the st-link wire and do it without debugging, the server itself doesn't workI try to find a way, but I don't know where the problem isIf the LED on the board blinks, it means it's dow...

ark2 by Associate III
  • 809 Views
  • 0 replies
  • 0 kudos

How to force a DRP usb PD3 port to source mode?

Hi, I am implementing a system with two DRP ports using an stm32g0 runnig a full USBPD stack. One of the ports is connected to a powerbank (usb pd v2). The other is connected to either a charger, which is used to power the system and charge the power...

Lvan .4 by Associate II
  • 1128 Views
  • 0 replies
  • 0 kudos

STM32G0 and FLASH_TYPEPROGRAM_FAST fail

Hello,I use a Nucleo-STM32G0B1 (512KB Flash).I would like to flash same data in fast mode, but the HAL_FLASH_Program() function ending with error. The HAL_FLASH_GetError() = 0x2A0 (PGSERR and PGAERR).Before writing I erase some flash pages.If I clean...

JTred.2 by Associate II
  • 6116 Views
  • 6 replies
  • 1 kudos

udp_client_on_stm32 board

hii , i really need some help :)i have the stm32h753 nuclio board and i am trying to run udp client on the board and my pc will be UDP_SERVER , i am using udp_echoclient_connect() and  udp_echoclient_send()  functions, that are inside the files tha...

abeba.1 by Associate III
  • 3331 Views
  • 1 replies
  • 0 kudos

Resolved! In a custom design, STM32H7 + USB3318 phy as a VCP device, if full-speed works but high-speed doesn't, what do you think would be the culprit?

In a custom design using a STM32H733vgt and a USB3318 phy, operating as a virtual com port device, full-speed works but high-speed doesn't work. If full-speed works but high-speed doesn't, what do you think would be the culprit?I'm using virtual com-...

Cannot ping using LWIP+FreeRTOS on Nucleo-F746ZG

Hi everyone, I'm new in this field. I was trying to integrate FreeRTOS with my TCP Server. While without FreeRTOS everything works fine, with FreeRTOS I cannot even make a simple ping. I'm looking everywhere for a solution but there aren't solutions ...

ZBru by Associate II
  • 2585 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.