STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F030F4P6 bootloader on PA2, PA3 possible?

I want to use hardware I2C (which is only available on pins PA9, PA10 on the STM32F030F4P6 in TSSOP20 case). That overlaps with the standard pins used in the bootloader code for USART1_TX and USART1_RX (AN2606 Rev 55, page 50). The alternative pins u...

BAren.1 by Associate II
  • 3347 Views
  • 5 replies
  • 0 kudos

recvfrom() is not working on stm32H7B3I-DK.

How to resolve recvfrom() issue on STM32_Network_Library. I'm using stm32H7B3I-DK board.FreeRTOSSTM32_Network_LibraryES_WIFI (BSP) When I tested UDP socket, sendto() was working.But recvfrom() was not working, it was blocked for ES_WIFI_MAX_SO_TIMEOU...

IChoi.2 by Associate
  • 1077 Views
  • 0 replies
  • 0 kudos

Resolved! I'm looking for STM32G Series product.

Hello?​As title, I want to know product with USB, FD-CAN, 2~3 DAC, etc.Problem is USB and HCLK are bound(using external clock), so that upper limit is determined to be low.(48, 96, 144 MHz in maximum 170 MHz)​For that reason, to ask the question, is ...

LSung.1 by Associate III
  • 3438 Views
  • 7 replies
  • 0 kudos

Resolved! I2S No operation what so ever.

I have 2 I2S ports. I have a masterclock from an external source.My clock config is set for external 24.576Mhz I2S clock.I have set up I2S1 in half duplex slave mode for an ADC. It is receiving data in DMA.I have setup I2S2 in half duplex master mode...

PCamp.2 by Associate III
  • 2966 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.