2022-11-22 4:33 AM - last edited on 2025-02-18 3:24 AM by Andrew Neil
How to resolve recvfrom() issue on STM32_Network_Library.
I'm using stm32H7B3I-DK board.
When I tested UDP socket, sendto() was working.
But recvfrom() was not working, it was blocked for ES_WIFI_MAX_SO_TIMEOUT.
The remote received an ICMP (Port unreachable).
This is my tested codes
/**
static void ecrio_udp_test(void)
{
int32_t sock = 0;
int32_t ret = 0;
sockaddr_in_t ServerIp;
sockaddr_in_t LocalIp;
net_ip4_addr_t addr;
net_ip_addr_t ip;
uint8_t received[1024];
uint32_t fromlen = 0;
memset((char *)&ServerIp, 0, sizeof(ServerIp));
sock = net_socket(NET_AF_INET, NET_SOCK_DGRAM ,NET_IPPROTO_UDP );
if (sock < 0)
{
printf("net_socket error=%d\r\n", sock);
}
printf("net_socket success\r\n");
ip4_addr_set_u32(&addr, NET_ATON_R("192.168.45.15"));
NET_IP4ADDR_PORT_TO_SOCKADDR(&ServerIp, &addr, 10000);
{
net_ip_addr_t remote;
remote = net_get_ip_addr(&ServerIp);
printf("remote ip = %s\r\n", net_ntoa(&remote));
printf("remote port = %d\r\n", 10000);
}
net_if_get_ip_address(&netif, &ip);
NET_IP4ADDR_PORT_TO_SOCKADDR(&LocalIp, (net_ip4_addr_t *)&ip, 20000);
printf("local ip = %s\r\n", net_ntoa(&ip));
printf("local port = %d\r\n", 20000);
ret = net_bind(sock, (sockaddr_t *)&LocalIp, LocalIp.sin_len);
if (ret != NET_OK)
{
printf("net_bind error=%d\r\n", ret);
}
printf("net_bind success\r\n");
ret = net_sendto( sock, "Hello!!", sizeof("Hello!!"), 0, (sockaddr_t *)&ServerIp, sizeof(ServerIp));
if (ret < 0)
{
printf("net_sendto error=%d\r\n", ret);
}
printf("net_sendto success sent=%d bytes\r\n", ret);
memset((char *)received, 0, 1024);
ret = net_recvfrom( sock, received, sizeof(received), 0, (sockaddr_t *)&ServerIp, &fromlen);
if (ret < 0)
{
printf("net_recvfrom error=%d\r\n", ret);
}
printf("net_recvfrom success received= %s, (%d) bytes\r\n", ret);
}
**/
Please find the attached. It is terminal log with ES_WIFI_DEBUG_MODE.
BR,
jee.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.