STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

usart interrupts vs freertos polling

My application has a low priority usart receive function - meaning that if characters are delayed it's no big deal. I've been using interrupts with a callback receiving one character at at time with a read always outstanding. I process flags and b...

Resolved! Is it possible to setup a USB-C only power connection (fixed CC resistors) while having the USBPD lib active?

I have set up the USBPD lib on my system to manage USB power delivery messages and set up power contracts in both the source and sink directions. Now that this seems to work well, I also want the system to work with a USB-C only power source (non-PD)...

Lvan .4 by Associate II
  • 2547 Views
  • 2 replies
  • 0 kudos

STM32 fail to receive data with DMA under RTOS

Hi guys,On STM32H7, try to receive data with UART in DMA normal mode under FreeRTOS, Tx works OK but receive nothing with keli5 (CubeMX setting as reference )I use HAL library,also tried LL library but not working.Already checked DMA is initialized b...

Rchan.1 by Associate
  • 1587 Views
  • 2 replies
  • 0 kudos

Clock configuration for STM32L4R9 with USB-FS - SDMMC

Hi,I would ask the community a suggestion for clock configuration.I should use the USB ans Mass Storage Class using the SD card by SDMMC interface as memory. This function is used for 5 to 10% of my device usage, so I would decrease the SYSCLK for po...

0693W00000QLc6mQAD.png
lukin by Associate III
  • 1108 Views
  • 1 replies
  • 0 kudos

I have a Lwip problem with SSI module.

The problem with the insert of the SSI tag, it is can insert only 920 characters but I need in 5 times more!If I change the "Lwip_httpd_max_tag_insert_len" It does not give an effect!Could someone tell me what is wrong?

DK.7 by Senior
  • 1055 Views
  • 0 replies
  • 0 kudos

STM32F7: ETH TCP checksum offload fails

Hello,ST's and all Ethernet experts, please.STM32F767, Nucleo-144, and custom boardno OS lwIP 2.1.3, IPv4 onlySTM32CubeIDEno ETH interrupts usedApplication: Industrial frontend, streaming "audio" data from SAIs via ethernet,at high data rates, for lo...

LCE by Principal II
  • 11158 Views
  • 29 replies
  • 0 kudos

Hi everyone, I am creating a project via STM32CUBEMX (V.6.4.0) for STM32G070 including AzureRTOS, however, I've encountered an issue using tx_thread_sleep function.

I've tried to create a simple project which includes 2 threads. Each thread toggles two separate pins respectively . To create a 10 ms delay, I am using tx_thread_sleep (TX_TIMER_TICKS_PER_SECOND is 100) . Everything works okay, however, I've noticed...

0693W00000WL0YNQA1.bmp
MR.16 by Associate
  • 2377 Views
  • 2 replies
  • 0 kudos

stm32 eth + lwip echo server ping

I'm trying to implement a server with eth+lwip with stm32, but it worked well when I debug it, but it didn't work when I tried to turn it off and on without debugging, so I'm trying this and that, but I'm not even pinging itIt says that the phenomeno...

0693W00000WKyKdQAL.png 0693W00000WKyLCQA1.png
ark2 by Associate III
  • 1628 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.