STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_UART_Transmit() and HAL_UART_Receive() API

I am using Nucleo board and Tera term for serial monitorI want to do simple addition programI want to take two values from serial monitor by typing (number + Enter ) and print back its additionExpect output on Serial monitor:enter value A : 5enter v...

RS009 by Associate III
  • 1437 Views
  • 1 replies
  • 0 kudos

Resolved! How To Run 2 UCPD ports on CMSIS V1

Hey allI am building an application using a STM32G071RB with a DRP1M1 as ucpd 0 and a USBDP1 (old SNK1M1) as ucpd 1 and new to the STM UCPD worldIn an attempt to start from a working base, I used the DRP1M1_DRP example project as a starting point. Th...

IOTkid by Associate II
  • 2899 Views
  • 3 replies
  • 0 kudos

Resolved! Having a hardtime to get SPI1 working on STM32H753ZI

Hi everyone, Hope all is well. I am trying to setup a basic SPI demo for the STM32H753ZI using the nucleo H753ZI just seeing if I can output my test word onto the MOSI line.The conditions in my SPI demo is as follows:MCU clocked at 400MHzSPI is set a...

0693W00000Y99iuQAB.png 0693W00000Y99ltQAB.png
CLeo.1 by Senior II
  • 3405 Views
  • 5 replies
  • 0 kudos

STM32H750XB USB I/Fs

Hi On STM32H750XB datasheet it says 2 x USBUSB OTG interfaces (1FS, 1HS/FS) .I configured the 1st port as FS, and the 2nd port as HS which connectd to external PHY (internal FS phy disabled) .I want to confirm that if the 2 ports can be used at diffe...

YHail.1 by Associate
  • 1176 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.