2023-01-25 1:01 AM
Hi
On STM32H750XB datasheet it says 2 x USBUSB OTG interfaces (1FS, 1HS/FS) .
I configured the 1st port as FS, and the 2nd port as HS which connectd to external PHY (internal FS phy disabled) .
I want to confirm that if the 2 ports can be used at different speed (1 as FS and 1 as HS) at the same time just for sure.
Thanks
2023-01-25 4:20 AM
Hello @YHail.1 and welcome to the Community :)
I confirm that both instances should work at the same time.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.