STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Query regarding Classb library

Hello Support TeamI am working on a single-phase EV charging product. and I have seen a certain metering solution on the STM website.For Communication and Application purposes, we selected the below MCU1. STM32G484QET62. STM32G473VET6 3. STM32G491RET...

USB Device interrupt transfer

I am using Nucleo-STM32 F767ZI board. I am to using interrupt transfer for sending data to PC(Host). But data is not getting displayed on game pad. When I use the  USBD_CUSTOM_HID_SendReport() function inside while(1) loop. it sends data and it gets ...

ATamb.2 by Associate II
  • 872 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L0538-DISCO Demo program

I recently bought the STM32L0538-DISCO board. I have seen the following video in youtube where you can see the functions of this board in full. Where can I find the source code for STM32Cube?On the info page of the board I have not found one that wor...

Daitec.1 by Associate II
  • 9100 Views
  • 16 replies
  • 0 kudos

I was trying to do file write operation on SD card and it worked for few days and now its giving "FR NOT ENABLED" error.

I was able to do file write operation on Sd card and usb both successfully , but after few days it is continuously giving me FR NOT ENABLED error, i formatted both devices and scanned if they might have malfunctioned it worked after formatting but no...

smore.1 by Associate II
  • 2022 Views
  • 3 replies
  • 0 kudos

ST example code has corrupted ETH RX Buffers

HI,I’m working on ETH and FreeRTOS on the STM32H745 Nucleo-144. I’ve read about various problems on this forum about using the ethernet as detailed belowhttps://community.st.com/s/question/0D53W00000rZ8ZvSAK/corrupted-eth-rx-buffer-in-stm32h7?t=16291...

0693W00000KbQfsQAF.jpg 0693W00000KbQgmQAF.jpg 0693W00000KbQiNQAV.jpg 0693W00000KbQiwQAF.jpg
CHossack by Associate III
  • 2836 Views
  • 4 replies
  • 1 kudos

Interface STM32H753 with LAN9303 Ethernet PHY

Hi,I've CubeIDE project for LAN9303 2 port ethernet driver. Followed the ST LWIP article and got the ping on the switch IC to PC.I have a problem with getting registers of lan9303. I guess the LAN8742 driver is doing minimal settings on the ic but wh...

umtkyck by Associate II
  • 2900 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.