2023-03-16 9:07 PM
I was able to do file write operation on Sd card and usb both successfully , but after few days it is continuously giving me FR NOT ENABLED error, i formatted both devices and scanned if they might have malfunctioned it worked after formatting but now i have to again and again format both of them to make the file operation work. Is there any solution for FR NOT ENABLED Error? This error says there is not enough space on logical drive whereas the card is completely empty and has enough space.
2023-03-17 12:35 AM
From description not really got much idea about your hardware or software implementation.
The file system is dependent on the block level DISKIO functions working properly.
2023-03-17 2:23 AM
Hello @smore.1,
I'm not sure if this helps but generally when you use 5V supply voltage, SD Card module works better. So, it's important to ensure that the power supply is stable.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-03-20 12:12 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.