STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Type C for charging and Power on first priority.

Hello , Is it possible to use USB Type C for charging and Power as First Priority when the Wireless Charging and battery is active respectively?Or a hardware switch or firmware is needed for this?Also please suggest the corresponding ST USB IC and wi...

PVaaz.1 by Associate III
  • 1889 Views
  • 1 replies
  • 0 kudos

Problem with I2C on STM32H7A3IIK6

Hi, i'm developing a project on STM32H7A3IIK6 [cortex M7] and i'm having a problem using the I2C peripheral with the ST HAL functions. I've initialized the peripheral and enabled the Event and Error Inpterrupt with TX and RX DMA and, sometimes, i hav...

Miglio by Associate II
  • 7423 Views
  • 15 replies
  • 0 kudos

Hello Everyone, I need to write sd card approximately 300 bytes per millisecond and in parallel get these data from another devise via spi, are there some suggestions how to do?

Hello Everyone, I need to write sd card approximately, 300 bytes per millisecond and in parallel get these data from another devise via spi, are there some suggestions how to do?I have tried to use SDMMC1 + Freertos, but I cant communicate with sd ca...

HHako.1 by Associate III
  • 2213 Views
  • 3 replies
  • 0 kudos

STM32F4 High Speed USB with LIBUSB

Hey everyone,I have been using the STM32F4 for quite some time now and have used the STM32F429 Eval1 board for developing a firmware that uses the external USB3300 PHY over ULPI to achieve high speed USB transfers in device mode with the CDC (virtual...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.