2023-05-02 8:57 AM
Hello ,
Is it possible to use USB Type C for charging and Power as First Priority when the Wireless Charging and battery is active respectively?
Or a hardware switch or firmware is needed for this?
Also please suggest the corresponding ST USB IC and wireless charging IC for this.
The power requirement is 3A@5V (max).
Regards,
P
2023-05-15 5:30 AM
Hello @PVaaz.1
Not clear to me what you want to do : charge battery through wireless AND type C at the same time ?
Cannot help you on a wireless solution.
On Type C side, 5V@3A : you don't need power delivery. So this is easy : no dedicated firmware is needed. Do you still need help on that ?
Regards,
Nicolas.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.