STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H747I-DISCO and ST Examples

After two days of trying, I decided to ask.I have this STM32H747I-DISCO and B-LCDAD-HDMI1. The examples that are from the site given below the board and consist of programming a single hex file work (STM32H747I-DISCO compiled demo binary), without th...

SFilc.1 by Associate II
  • 4091 Views
  • 5 replies
  • 0 kudos

Resolved! Get value from a buffer

I have an ADC input that is read continuously and put in a buffer by the help of DMA. This is my buffer:uint16_t adc_buf[ADC_BUF_LEN];        //ADC_BUF_LEN = 1The value in the buffer is replaced continuously by the NEW sampled value from the ADC.I wa...

HØdeg.1 by Associate
  • 4008 Views
  • 4 replies
  • 0 kudos

STM32H7 UART DMA recieve issue

Hello,I have been trying to establish the UART communication using DMA. To implement that I referred to https://community.st.com/t5/stm32-mcus-products/stm32h7-uart-dma-receive-unknown-length-of-data/m-p/86869#M11292 post. I am trying to implement DM...

HDesa.1 by Senior
  • 3779 Views
  • 4 replies
  • 1 kudos

Changing Timer Capture Compare from Timer ISR

I am trying to change the PWM duty cycle of timer3, channel 1 from the period elapsed ISR of timer 6. This seems to cause the chip to crash. I can confirm that:- timer6 is properly configured and interrupt fires appropriately.- timer3 is properly con...

Split .BIN in multiple regions

Hi,I want to split the .BIN file because it is too big... Here is the size of the files :.BIN size : 2.13 Go.HEX size : 30.5 Mo.ELF size : 11.4 MoHere is the memory used :I am using an USB flash drive to update my system program. I know I need to spl...

0693W000006EImtQAG.png
MMerc.1 by Senior
  • 5683 Views
  • 6 replies
  • 0 kudos

MAC/MDIO Issues with STM32H7 Emcraft SOM

Hi STM32 Community,I'm using a SoM with the STM32H750, made by Emcraft. My goal is to set up Ethernet using the standard HAL library alongside lwIP. However, I've hit a snag with the MDIO communication to the PHY(a Waveshare LAN8720 board).Based on t...

MDIO_MDC_1.png MDIO_MDC_2.png
Sonic_TS by Associate
  • 2821 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.