STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FATFS and USB integration

 I am currently working on a project that involves integrating USB functionality for data transfer and data logging on an STM32F407VG micro-controller. Specifically, I want to log data files on an SD card and enable the user to download these logged ...

PLL: anybody using the internal PLLs as VCO for audio?

Hello,I was just porting a F767 design to an H723-Nucleo, and found out that this H7 Nucleo is using its ST-Link's HSI as a clock source to the H723 at 8 MHz. With the usual terrible HSI quality, which showed itself in low quality SPDIF TX and PTP sy...

LCE by Principal II
  • 2459 Views
  • 3 replies
  • 0 kudos

STM32F407 LWIP TCP Server Rx Stalling

Hello, I'm working on a STM32F407 LwIP acting as a TCP server with a bare winsock based client on Windows 10.The project is derived from CubeMX V1.27.1 with the tcp_echoserver.c module creating and communicating to the client.After a few transfer of ...

Resolved! Differential ADC

If this is not the right section of the forum to ask this question, I kindly ask you to move it to the correct one. Thank you!I need an ADC with differential input but I only have STM32F407 (which doesn't have it). I was thinking of sending the diffe...

luke514 by Senior
  • 4614 Views
  • 3 replies
  • 0 kudos

ADC

Hello everyone I am using two channels of ADC in the stm32f429 board and collecting some chunks of data for further processing. I want to collect data once the zero crossing is detected currently I'm using zero crossing detection c code is there any ...

harry123 by Senior II
  • 1053 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.