STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DCMI Crop feature

Hi all, I recently started learning about st-controllers and I am stuck in this, any help would be greatly appreciated.I am working with stmf746, I wanted to crop the captured image with DCMI crop feature, I am configuring crop window size and offset...

lglad by Associate
  • 2840 Views
  • 3 replies
  • 1 kudos

PWM phase shift for dual active bridge

I have a dual active bridge and I am supposed to do leading and lagging phase shift to achieve that. This needs to be a precise shift to the lowest degree of 1. I am using an STM32F429. This is the logic I am using:HAL_TIM_PWM_Start(&htim3, TIM_CHANN...

Gaia by Associate
  • 982 Views
  • 0 replies
  • 0 kudos

USB CDC works on STM32G431 but not STM32L151

Hi, I am trying to setup USB CDC as virtual COM port on STM32L151. I just enabled it through cubeMX and connected the wires. Windows keep saying device not recognized.I just did the exact same thing with STM32G431. An empty project with just USB CDC ...

HKaze.2 by Associate
  • 1754 Views
  • 2 replies
  • 0 kudos

Resolved! Upgrade from STM32L432KB to STM32L432KC

Hi Everyone,I'm upgrading our firmware from STM32L432kb with 128k flash memory to STM32L432KC with 256k flash memory. both micro controllers are  exactly the same except for the flash memory size difference. To accommodate this change I changed my co...

RTOS Task management "architecture"

Hello everyone.This is more of a general RTOS question regarding the approach of task management. I've got everything pretty much working but im certain there is a better solution than mine. I'm using FreeRTOS with the CMSIS v2 wrapper.Background:The...

XD by Associate III
  • 1983 Views
  • 0 replies
  • 0 kudos

strange long eth transmission

I am using  STM32H735AGI with freertos + lwip + no dcacheI have an udp echo server on the device and a udp echo client in python that runs on the pcThe client sends messages with a length of 3 TCP_MSSIn the following logs the first number is the tick...

mzenn.280 by Associate II
  • 1323 Views
  • 1 replies
  • 0 kudos

FDCAN Filter problem in Classic Mode STM32U575I

Hi,I am working using FDCAN as Classic CAN 2.0B, in STM32U575-EV kit.I am facing issue with FDCAN filtering with Classic Mask mode. There is two cases of filter configuration explained below, in first case it is working as expected but in second case...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.