2023-11-06 8:13 AM
My project uses H7 MCU
When I use the USB host I try to write to the USB device, this works OK if I do not write more then 13 characters to a line any more and the data is not written to the file but the file is still created. The below code writes 1000 lines to a text file.
uint8_t wtext[] = "\n hello world!1"; // this works
// uint8_t wtext[] = "\n hello world!12"; // this does not work
fresult = f_mount(&USBHFatFS, (TCHAR const*)USBHPath, 1); // mount usb stick
fresult = f_open(&USBHFile, "1:/USBHost.txt", FA_CREATE_ALWAYS | FA_WRITE); // create file
f_close(&USBHFile); // close to ensure the file is created
for(int i = 0; i<1000; i++)
{
fresult = f_open(&USBHFile, "1:/USBHost.txt", FA_OPEN_APPEND | FA_WRITE); // open the file
fresult = f_write(&USBHFile, wtext, sizeof(wtext), &byteswritten); // write the data
f_close(&USBHFile); // close the file
}
fresult = f_mount(NULL, (TCHAR const*)USBHPath, 1); // unmount usb stick
I have attached the CubeMX file as a txt, the uploader did not like the file format :astonished_face:
Please can you help me unsderstand what I may change to overcome this.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.