STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Overwrite Hardfault_Handler with a custom assembly implementation in STM32CubeIDE generated code

Hi Community, I am trying to define a custom Hardfault_Handler definition in the assembly to overwrite the default template given in the stm32xxxx_it.c in the STM32CubeIDE generated code. When the definition is put under custom.s and added to the ass...

Resolved! 16 bit ADC interface

HiiI'm interfacing External adc with stm32f429I want to read 16-bit parallel data from ADC and connected16 lines from ADC to GPIOA GPIOA->IDRhow the data is stored in IDR and how to access the input data register continuously for every sample. Thank ...

harry123 by Senior II
  • 1799 Views
  • 2 replies
  • 2 kudos

Transmission of a matrix on CAN bus

Hi, I have an STM32H723ZG and I want to transmit a matrix in which I stored some measured data on a CAN bus. I can use the following function only writing the pointer to the matrix in "pTxData" or I have to segment the matrix?HAL_FDCAN_AddMessageToTx...

ECiot.1 by Associate II
  • 1395 Views
  • 1 replies
  • 0 kudos

Send large chunks of data via BLE

Hello,I want to use the SensorTile.box to collect IMU data over BLE. I tried modifying the BLESensors source code to suit my requirements (by increasing the characteristic size etc.). But the ST BLE Sensor app doesn't seem to support this. I only rec...

Flare by Associate II
  • 1137 Views
  • 0 replies
  • 0 kudos

lis3dsh pedometer

I have a stm32f407vg development board. I want to make a pedometer project with the lis3dsh sensor on this development board. I couldn't find enough resources and examples. I need to make this project in C.Can you help me please? 

Resolved! STM32L4 SDMMC + FATFS

Hi, I would like using SD card with FATFS and read/write to SD card.If i have bare-metal FW without DMA template enable it is work.But if I enable DMA template f_mount, f_open return FR_OK but f_write, f_read Disc_error.I setted in CubeMX SDMMC1- SD ...

lorant124 by Associate III
  • 2887 Views
  • 2 replies
  • 1 kudos

STM32 Cube IDE: Reset_Handler() at 0x80021e0

Hi STM team,I am using the STM32WL55CCU6 MCU on a custom PCB project. I actually have two of these. One is working as a master, while the other operates as a slave. My slave device is working properly, but the master is not. Problem Statement: When d...

Reset_Handler.PNG main_warning.PNG installed_software.PNG
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.