2024-01-22 5:58 AM
I have two doubts kind clear it.
1) I want remove and dont want to build stm32mp135f-dk-a7-examples.dtb, so where can I remove example dtb which is selected from extlinux.conf?
2) I want to mount my desired partition where and how it can be mounted?
2024-01-22 6:08 AM
To remove the building of stm32mp135f-dk-a7-examples.dtb, you'll need to modify the configuration files. I think you'll get more helpful responses if you share more details.
2024-01-23 1:57 AM
Dear sir,
1) If you see during boot, we have option to select different dtb like stm32mp13f-dk.dtb and stm32mp135f-dk-a7-examples.dtb. I just want my kernel should start with stm32mp13f-dk.dtb and there should not be any option to select any other dtb. But when building rootfs, this file comes automatically. I just want to remove all example dtb from yocto build so that it dont come in /boot folder of rootfs.
2) I want to mount partition like user2.ext4 and vendor2.ext4 in my hardware, how is that possible using yocto build process?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.