STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB PD Stack Library with EPR

Hi, I use the USBPD Middleware to implement a PD Port with a G474RB. This is functional. Now I would like to implement USB-PD EPR. I cant find any settings that would make cubeMX use the EPR version of the stack, the cubeMX inputs are further limited...

janik by Associate II
  • 141 Views
  • 4 replies
  • 0 kudos

Resolved! Camera demo project for testing TFT preview

I am using the STM32H7B3I-EVAL board. I checked STM32CubeH7.Since the board supports camera (DCMI) .Any camera demo project for testing LCD previewAvailability of prebuilt binaries (.hex / .bin / .elf) for quick hardware testingGoal: quick validation...

stm32h5xx Ethernet MDIO clause 45

Hi,I working with nucleo-h563zi.I try to use MDIO as Clause 45, copy HAL_ETH_WritePHYRegister, HAL_ETH_ReadPHYRegister and change it's to fit for Clause 45.#define ETH_MACMDIOAR_MOC_ADD_Pos (2U) #define ETH_MACMDIOAR_MOC_ADD_Msk ...

shonz_0-1780394520247.png
shonz by Associate
  • 94 Views
  • 1 replies
  • 1 kudos

STM32U575VGT: Autonomous SPI reading

I have a project where a STM32U575VGT must convert a SSI multiturn encoder value into a parallel single turn value for GPIO output. The SSI values are 3 bytes long, and it would be best if the CPU is only interrupted when the last 2 values differ. I ...

Roth.Ian by Associate III
  • 486 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.