cancel
Showing results for 
Search instead for 
Did you mean: 

STM32N6570-DK | VENC_SDCard_ThreadX | Using exFAT

dksmith
Associate II

I have been modifying the VENC_SDCard_ThreadX example to read in raw data through pipe0 with success. However, my bottleneck appears to be the SD card write speed; I understand that this example was designed to write compressed h.264 files - and it looks like it only writes at around 320 kB/s.

Since I am capturing much more data, I would like to use exFAT instead of FAT32, and write to a UHS I card at max speed (SDR104). I defined FX_ENABLE_EXFAT within fx_user.h, but it I am still unable to write to an exFAT formatted card.

fx_media_open() passes just fine, but upon inspection it appears that the available clusters always is 0. Am I missing any steps? Any insight would be appreciated.

5 REPLIES 5
Saket_Om
ST Employee

Hello @dksmith 

Could you share your code please, then we can assist you more effectively. 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om
dksmith
Associate II

Hello,

To test writing to exFAT I have just been running the unmodified VENC_SDCard_ThreadX example code. I made sure FX_ENABLE_EXFAT was defined in fx_user.h. This was my only edit. 

dksmith
Associate II

I have also attempted to use fx_media_exFAT_format() to format the card for exFAT upon initialization, but no change. It seems like the cluster size always starts at 1 and then becomes zero.

Hi @Saket_Om and @dksmith 

Thank you very much for this discussion.

We're looking at using STM32N6x7 to receive video from ST image sensors via MIPI CSI-2, do h.264 encode and write it to a FAT32 or exFAT filesystem on SD for a new open source wildlife camera for conservation of endangered dormouse species.

It would be great to know if you were successful in adapting this example to write to exFAT?

Thank you very much!

Will

Saket_Om
ST Employee

Hello @dksmith 

In order to ensure the application functions correctly with the ExFAT file system, the following updates must be implemented:

1. Defined Symbols (Preprocessor)
Add "FX_INCLUDE_USER_DEFINE_FILE" to project configuration to force the compiler to include fx_user.h, ensuring exFAT configurations are applied in the project.

2. Set #define FX_STM32_SD_DEFAULT_SECTOR_SIZE 512 in fx_stm32_sd_driver.h (Exfat requires min sector size 512)

3. Since the SD driver uses DMA, the memory buffer must be properly aligned and cacheable (in a cacheable section) to avoid data corruption.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.