STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4Q5AGIx Hyperbus PSRAM Issues

We are using a STM32L4Q5AGIx device with Hyperbus PSRAM IS66WVH8M8BLL chip on a custom board.  We are having a number of issues getting the RAM to work corectly on Port 2 and right now are isolating it to reading any of the 4 internal registers, ID0,...

hyperbus_ScopePic.png
BComp by Associate
  • 1464 Views
  • 1 replies
  • 1 kudos

Resolved! stm32h743zi WINUSB(HS) ISSUE

I AM USING STM32H743ZI IN USB_HS IN CONTROLLER BUT WHEN I CONNECT USB CABLE TO CPU IN DEVICE MANAGER IT DISPLY winUSB BUT IN zadig software not install the libusb driver it seen the driver not install so how how to solve this problem suggest me 

SITARAM by Associate III
  • 1657 Views
  • 2 replies
  • 0 kudos

stm32h563 Azure Netx Multihome Support

Hello,I have created and executed a TCP server project with Azure NetX library using Ethernet. Additionally, I need multihome support in this project. I want multiple clients to connect to a device with a static IP. Can you assist me with this?Best r...

Eakyo.1 by Associate III
  • 3492 Views
  • 4 replies
  • 0 kudos

Resolved! HS USB MSC as Device --> formatting error on Host

Hi,I am trying to set up a basic HS USB MSC project on a custom board with an STM32F723.The project is based on these tutorials from ST, the only difference is, that I'm using USB HS and not USB FS.https://www.st.com/content/st_com/en/support/learnin...

CObri1_0-1707986829194.png CObri1_1-1707986910415.png CObri1_2-1707986995601.png CObri1_3-1707987560888.png
CObri.1 by Associate III
  • 7002 Views
  • 6 replies
  • 2 kudos

Resolved! USB PD Development Environment

X-NUCLEO-DRP1M1 と NUCLE0-G071RB を持っています。USB 開発には x-cube-tcpp を使用します。ただし、構成ファイル (.ioc) を使用すると、コード生成があることに気付きました。設定ファイル(.ioc)を使用したUSBPD設定ファイル(.ioc)を使用してUSBPD用のソフトウェアを開発することはできますか?サンプルプロジェクトはありますか?

forst by Associate III
  • 2178 Views
  • 2 replies
  • 1 kudos

Resolved! USBC PD TCPM on the STM32U5

Hello,I have an application that uses the TCPM/TCPC architecture, with a STM32U5 acting as the port manager, and the FUSB307B as the port controller. I want to use the USB-PD middleware stack for the policy engine, however, when looking at the availa...

rward by Associate
  • 6655 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.