STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32f439 freertos lwip stuck

Hi, i have build up a basic freertos and lwip setup. I just have one user task running. I start a sntp to get the time and wanted to print the time in that task. But it does not reach there.I get stuck. I'm using the cmsis v2 i recently upgraded the ...

MOtto.2 by Associate II
  • 2074 Views
  • 2 replies
  • 0 kudos

Resolved! How can b-cams-omv be connected to STM32F746G-DISCO?

Hello,I am trying to connect b-cams-omv(ov5460) camera module into STM32F746G-DISCO board.However I can not find an official sample code examples.I downloaded FP-AI-VISION1_V3.1.0 SW package from ST web-page. When I unzipped it. it found in Drivers\B...

Sejinoh by Associate II
  • 1393 Views
  • 1 replies
  • 0 kudos

Problem with "HAL_UARTEx_ReceiveToIdle_DMA"

Hi,I am using the HAL function "HAL_UARTEx_ReceiveToIdle_DMA" as follows:void HAL_UARTEx_ReceiveToIdle_DMA(UART_HandleTypeDef *huart, uint16_t Size) {//my actionsHAL_UARTEx_ReceiveToIdle_DMA(peripheral, buffer, COMMAND_MAXIMUM_LENGTH);__HAL_DMA_DISAB...

areyzummo by Associate II
  • 4843 Views
  • 7 replies
  • 2 kudos

Ethernet issue after power cycling of STM32H723ZG

I'm having the same problem with STM32H723ZG, with our own board, Ethernet can only be connected after using ST link to download the code (either by "debug" or "run"). After power cycle the board, it won't connect anymore, reset button didn't help.  ...

ETong.1 by Associate II
  • 8253 Views
  • 10 replies
  • 0 kudos

Resolved! STM32H743ZI2 TIMER calculation

Im using stm32h743zi2 microcontroller and , cortext M7 processor , so i need prescalar value and period values of TIM5 for 80milli sec . here im using main clock is 400Mhz and timer bus clock is 200Mhz . please can anyone suggest me a flexible soluti...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.