STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Flash test issue

Hi In previous posts, I encountered the similar problem, but I did not find an accurate answer.Please advice me on this issue. 

VDD pin connection of STUSB1600

Hi, I am trying to use STUSB1600 as a front end interface to my USB Type-C connector and interface it with STM32L4R9 series microcontroller. It is a dual role type application but with no power delivery. Unable to understand why VDD of STUSB1600 is c...

MoniR_1-1711709267257.png MoniR_2-1711709502506.png
MoniR by Associate
  • 2787 Views
  • 4 replies
  • 2 kudos

Resolved! STM32H730 PA10 going high when turning on USB HS PHY

Hi all,We are using an STM32H730IBK6Q.PA10 is not configured and STM32CubeMx generates code that initializes the pin as "Analog" as expected.Now if we enable USB (specifically, when setting `USBx->GCCFG |= USB_OTG_GCCFG_PWRDWN;`), that pin goes high,...

jri_0-1712234914627.png
jri by Associate II
  • 3051 Views
  • 4 replies
  • 2 kudos

Firmware Update via UART boot commands

Hi guys, I have a nucleo-l073rz and am developing software for it with iar ewarm. So far everything is working well (programming and flashing via the st-link programmer). In the future, however, I would like to do firmware updates via the serial inte...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.