STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

usb using in stm32h743zi

when i connected usb connector in stm32h743zi,  that time what function working usb connector and if i remove usb connector then what function going to usb connector ,give me that function i remove usb

SITARAM by Associate III
  • 1524 Views
  • 2 replies
  • 0 kudos

Safety Test Library : rom test fail issue

I'm using the STM32F767 MCU and Keil compiler. The Keil version is Fusa 16.2. When applying the STL library in the Keil compiler environment, a rom test failure occurs.STL version is 4.0, and it was applied as in the guide document, but STL_Lib respo...

제목 없음.png
MLee.14 by Associate
  • 1184 Views
  • 0 replies
  • 0 kudos

Deferred Debugging Activity - Debugger Freezing

I am working on a project for an OEM's proprietary board firmware package (developed/baked from scratch), which has been developed from scratch with reference to two OEM's proprietary board firmware packages (fully baked). Thus, we may call this as c...

lbs by Associate
  • 2435 Views
  • 2 replies
  • 0 kudos

pBuf size and memory allocation.

BackgroundNUCLEO-H723ZG BoardFreeRTOS + LWIPUsing netcon with netbuf in its own task to receive packets as follows,IGMP Groups, receiving sACN packets (638 bytes per packet at 5us spacing), each group you join adds a packet, there is a 40ms gap betwe...

Shaun_82 by Associate
  • 2467 Views
  • 1 replies
  • 1 kudos

USB AND Ethernet both are using in my divice

I AM USING A STM32H743ZI CONTROLLER  BOTH USB AND ETHERNET ON WORKING BUT SOME TIME I RUNNING ON ETHERNET DEVICE THAT IS WORK OK  BUT I START WORK ON USB THAT TIME I CONNECT USB DEVICE NOT PROPER WORK ,SO I HAVE REQURED A FUCTION WHEN USB DIVICE CONN...

SITARAM by Associate III
  • 1246 Views
  • 1 replies
  • 1 kudos

Resolved! [stm32F411RE] Turning on LD2 through C, not working!

Hi ST Community! Warning, this is about to be a long one :) I have tried following the LED on step by step, but for my board. In this instance, the LED I am flashing is LD2 on my board which is connected to pin D13, based on the schematic below (whic...

aeaefbay_7-1712811987963.png aeaefbay_8-1712811999985.png aeaefbay_9-1712812009327.png aeaefbay_10-1712812020895.png
aeaefbay by Associate
  • 3306 Views
  • 3 replies
  • 1 kudos

Resolved! IAR 8.50 not discern STM32C0XX series chip

HI Guys,Sorry to bother you... Now I was working use STM32C0XX series chips, my development tools is IAR8.50, and find that IAR8.50 can't show STM32C0XX series chip, I had check some data: someone said should upgrade IAR FW, others said I should add ...

gavin3_0-1712804660484.png
gavin3 by Associate II
  • 1778 Views
  • 2 replies
  • 2 kudos

Resolved! STM32U595 USB pins do not work as GPIO

Hello ST experts I found the same problem as previous post  https://community.st.com/t5/stm32-mcus-embedded-software/stm32f072xb-gpio-issue-usb-pins-do-not-work-as-gpio/m-p/151104#M8715  But for stm32u595, I can not find the similar register USB_CNTR...

Yang Yang by Associate III
  • 4291 Views
  • 7 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.