STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H QSPI LL Driver

Hello,I'm trying to implement the QSPI interface to a micron device utilizing the OSPI hardware with LL kinda of driver (It's not available so I tried to write it by myself). I configured the OSPI and OSPIM registers and from signals that I see on my...

OGhad.1 by Associate
  • 1787 Views
  • 1 replies
  • 0 kudos

HAL_RCC_OscConfig function takes too much space

Posted on November 15, 2017 at 11:09Hello After I face some fitting to flash problem I saw my largest function is HAL_RCC_OscConfig.I thouht a function that writes static variables to registers should be smaller. Am I doing something wrong or is the...

mtp without threadx

Hello,I want to use the USBX MTP stack on a stm32u5 without threadx. The configuration in stm32CubeMx worked fine but when i run the programm, i get UX_FUNCTION_NOT_SUPPORTED from this location: UINT _ux_device_class_pima_initialize(UX_SLAVE_CLASS_C...

codgen by Associate
  • 1855 Views
  • 2 replies
  • 0 kudos

STM32U5 series bank swap not working

First post, please let me know if I've made any mistakes in asking my question.I'm trying to write a bootloader for a device using a STM32u585ZIT chip. When booting, it will read a partition table saved in flash to determine if it will boot from part...

HParsons by Associate
  • 2154 Views
  • 1 replies
  • 0 kudos

STM32H7 - USB MIDI

Hi, I'm working on a project which requires USB MIDI functionality. I looked into a couple of videos where USB MIDI implementation was done on other boards, but when I try to do the same on mine it's not working. I'm using a NUCLEO board (H755ZIQ), I...

isaacjack by Associate II
  • 2075 Views
  • 1 replies
  • 1 kudos

Resolved! ETH_SetMACConfig and ETH_SetDMAConfig function query

Hello,Just wondering if anyone knows the reason for the duplicate writes to the following registers in the HAL Ethernet code please?ETH->MACCRETH->MACFCRETH->DMAOMRETH->DMABMRIn the example shown below (from HAL code) the DMA0MR register is written t...

###### by Senior II
  • 3883 Views
  • 7 replies
  • 2 kudos

How to reading wakeup flag?

I want to know which Wakeup pin or Reset pin wakes up the microprocessor that enters standby mode. I have 2 wakeup pins.I am monitoring SR1 and SR2 variables with Live expression in Debug mode, but when I wake up from standby mode, the value of the v...

Macun by Associate II
  • 2903 Views
  • 3 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.