2024-04-28 7:41 PM - last edited on 2024-04-30 4:01 AM by Amel NASRI
Hi,
I'm using a nucleo board with stm32h755zi chip for prototyping a MIDI device. I am trying to get it working as both CDC and MIDI device via USB. I was able to achieve this using I-CUBE-USBD-Composite but there is a minor problem with the implementation. What i've done so far is, I created a HID + CDC composite class and i changed the HID descriptor to MIDI descriptors. So by using send report function i can send MIDI notes and by using CDC transmit function i can send serial data. Before i added MIDI descriptors i was able to transmit CDC data with just a single channel. That is i set _USBD_CDC_ACM_COUNT as 1. But when i added MIDI descriptors my CDC transmit stopped working even though i was able to detect a serial monitor. To solve this what i did is, i changed _USBD_CDC_ACM_COUNT to 2. Now i can see two serial ports and the second port works fine whereas the first channel is still not working. When i look at the code second channel has different end points
Thanks,
Kiran
2024-05-02 8:03 AM
Hello Kiran,
I-CUBE-USBD-Composite is not part of ST software offer, seems that package uses a customized middleware based on ST USB device library and the issue you faced seems not be linked to ST software
Regards,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.