STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ETHERNET STOP WORKING AFTER 5 DAY

I AM USING A ETHRNET ON STM32H734ZI  BUT ETHERNET CONTINUE WORKING FOUR DAY  ON MY DIVICE AFTER STOP MY DEVICE WORKING SO I CAN NOT FIND MY SOFISTICATED SOLUTION IN ETHERNET  PLEASE GIVE MI SOLUTION

SITARAM by Associate III
  • 1593 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H7, end of period interrupt

Hi, I'm using a timer to create a software delay on a high prio task (HPTask with FreeRTOS).The MCU used is STM32H755ZI.My target is:use a timer and arm an interrupt which duration will be 250 usec;suspend the HPTaskon the timer END PERIOD interrupt ...

lonejack by Associate III
  • 1495 Views
  • 1 replies
  • 0 kudos

stm32 lwip dhcp

I am using nucleof439 with lwip. I use DHCP to get ip address. Is anyway to detect IP address to be set? I notice there is two thread, "tcpip_thread" and "EthLink", I don't know which one is good for user to get ip address, also struct netif is local...

yang hong by Associate III
  • 1880 Views
  • 1 replies
  • 0 kudos

Resolved! input capture method using stm32f303RBT6 Mcu

Hi Team,We use stm32f303Rbt6 microcontroller. I need a output for Input capture, I am using two timers. I generate pulse for Tim1(1khz) and I set for Tim2 for input capture mode(input capture direct mode). TIM1 generate the pulse for continuously(1kh...

Screenshot (24).png Screenshot (25).png
mrsmile by Associate III
  • 3138 Views
  • 4 replies
  • 1 kudos

Resolved! STM32C01x RTC initialization Timeout error

I am working on firmware with stm32c011f4u6 mcu. When the program is operated, a timeout error occurs after falling into the infinite loop of the function below. HAL_StatusTypeDef RTC_EnterInitMode(RTC_HandleTypeDef *hrtc) { uint32_t tickstart; H...

KenLee by Associate III
  • 1796 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.