STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SBOM for STM32 firmware project

Hi,I have this toolchain and need to generate a SBOM:STM IDE v1.18STM IDE GNU Tools for STM32 13.3.Rel1STM32Cube FW_L4 V1.18.1, specified in `\*.ioc` fileSTM32_USB_Device_Library (v2.0_Cube)STM32CubeMX 6.14.0FreeRTOS (10.3.1)How could I turn this int...

dgep by Associate II
  • 665 Views
  • 3 replies
  • 1 kudos

uart data mismatch

I am using stm32f407 and stm32wb series for sending the data usimg uart.first i send th data using the stm32wb uart to the stm32f407 uart the data is correctly sent.After receiving the data i will return the data back to the stm32wb from the stm32f40...

TejasK by Associate III
  • 1035 Views
  • 10 replies
  • 2 kudos

Resolved! Nx_WebServer example on STM32N6570-DK board

I tried in use Nx_WebServer factory example written for STM32N6570-DK board. Finally I compiled (without error) and run the project but nothing (except single step) worked.It never got IP address from DHCP.The Green LED is not blinking.With static IP...

Louie88 by Senior II
  • 362 Views
  • 2 replies
  • 1 kudos

Resolved! STM32H563 / STM32Cube FW_H5 v1.6.0 regression: `ADC2_INP0` broken by `LL_ADC_EnableChannel0_GPIO()` change, reference manual unclear

I found an ADC regression on `STM32H563RG` after upgrading from `STM32Cube FW_H5 v1.5.1` to `v1.6.0`.Setup:- MCU: `STM32H563RG`- Old package: `STM32Cube FW_H5 v1.5.1`- New package: `STM32Cube FW_H5 v1.6.0`- CubeMX: `6.17.0`Symptom:- I sample multiple...

KaiY by Associate III
  • 368 Views
  • 1 replies
  • 3 kudos

Resolved! USB device not recognized

Hi, I have created a project in STM32CUBEIDE for STM32U575ZITQ for USB CDC. I am getting an 85 | HAL_PCDEx_PMAConfig((PCD_HandleTypeDef*)pdev->pData , 0x00 , PCD_SNG_BUF, 0x18); | ^~~~~~~~~~~~~~~~~~~ | HAL_PWREx_PVMConfig ../USB/Core/Src/usbd_conf....

APD by Associate II
  • 478 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.