STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F767ZI: Hard fault with FreeRTOS mutexes + DMA I2C

My setting is a Nucleo F767ZI board with a IKS01A2 shield. I created a FreeRTOS project that periodically queries the temperature sensor, calculates an average of temperature data, and prints the temperature on the UART. It has three threads that wor...

PB1 by Associate III
  • 3471 Views
  • 5 replies
  • 5 kudos

STM32H743 Internal CPU Temperature

 Hello, I am trying to calculate the internal CPU temperature on an STM32H743, When reading the internal CPU temperature sensor using ADC3 IN18 (internal temperature), I get a very high value (~731C)The formula I'm using is the following :Temperature...

anasba by Associate II
  • 8808 Views
  • 13 replies
  • 3 kudos

Resolved! a bug about using execution profile kit in threadx

Hi, i'm trying to use execution profile kit in threadx. I use STM32H750VBT6 and STM32CubeIDE1.12.0firstly, i use stm32cubemx to generate the code include threadx. I can't find execution profile file in the code. So I get tx_execution_profile.h and tx...

xixi by Associate II
  • 3328 Views
  • 4 replies
  • 2 kudos

Resolved! How do I jump from application code to bootloader without toggling the BOOT0 pin on STM32H745?

I followed this article by @Khouloud GARSI​ and was unable to get the function to jump to the bootloader working. The application seems to freeze after I execute the function given in the article and the bootloader doesn't ACK my messages until I re...

USB host MSC read sector count

Hello everyone.I am working on a project which needs low level access to USB mass storage class such as reading sector size/count of an attached storage device but thus far I could not get anything out of my board which is nucleo-f446re.I have initia...

STM32F4 Usb fails to work only when in debug mode

I am working on a basic USB FS HID device on an STM32F411 Discovery Board, the USB code is the only code on the board. When I run the code from the STM32CubeIDE, the device fails to enumerate and Windows says "Device Not Recognized". I have no breakp...

MB.2 by Associate III
  • 5610 Views
  • 8 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.