STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SMT32L4 CAN bootloader not initializing

I have a STM32L431 that jumps to the bootloader using a software jump to 0x1FFF0000.I verified that the PB8 and PB9 pins are used on my system and I also have a 8MHz crystal soldered. I let the bootloader run then I send a 0x79 standard identifier wi...

bareil76 by Associate II
  • 4413 Views
  • 2 replies
  • 0 kudos

Resolved! Custom HID Receive data

Hi,I'm using Custom HID class for sending MIDI messages by editing the descriptors. I am using sendReport function for sending MIDI messages, I want to receive MIDI messages as well. I was wondering whether there is any function to receive messages i...

kps98 by Associate III
  • 2209 Views
  • 2 replies
  • 1 kudos

Resolved! OTA modular update STM32F446ZET6 with FreeRTOS

Hi all,I need to perform a modular update in my f446 board for my project.The board is running a FreeRTOS, and the idea is to only modify the content of one task without affecting the content of other tasks. For doing this, every task calls its funct...

jaumas43 by Associate II
  • 3802 Views
  • 6 replies
  • 1 kudos

Unable to download any software

Hi Guys, I have been trying to download FP-AI-PDMWBSOC, I always get this message "This software is not available for download.". It is not only software that gives me this issue. Does anyone have a fix?    

KQ by Associate
  • 2367 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 Nucleo-H723ZG board HTTP server netconn ST example, get hard fault exception when I disconnec

Hi All, I have a STM32 Nucleo H723ZG development board and running CMSIS RTOS v2 and HTTP server with netconn  on it. The project is an example provided by the ST and it is available in STCubeMX. everything works fine until I disconnect the Ethernet ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.