STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

sdcard not working

we are using stm32f103c8t6 and stm32f407vet6 microcontrollers. we were able to communicate with sandisk and other brand sdcards but hp sdcard (Class 10, UHS-I, U1) is not communicating . hp sdcard working with card reader and we have formatted in FAT...

sdcards hp.png
Sansel by Associate
  • 1980 Views
  • 3 replies
  • 1 kudos

Resolved! USB virtual COM port does not work when debugging

Hello, I am trying to debug my vcp application (uses STM32F103CBT6), but when I start a debug session the COM port does not work. When not debugging, just uploading a new code, the cdc communication only works after a power reset. I modified my custo...

PSzab1_0-1716736470675.png PSzab1_1-1716737814331.png PSzab1_2-1716737848410.png PSzab1_3-1716737879365.png
PSzab.1 by Associate II
  • 3890 Views
  • 5 replies
  • 2 kudos

Variable value not the same as in memory (STM32H7)

Hi!I'm working on a STM32H7 running with FreeRTOS.I'm facing a quite particular bug. One specific variable, which is basically a counter, sometimes get its value corrupted.This happens inside an specific task, which is actually quite simple, and over...

TVare.1 by Associate III
  • 1899 Views
  • 2 replies
  • 0 kudos

Resolved! cant ping nucleo-h723 dev board using lwip

HiI am trying to develop a board based on ethernet connection. I have bought a nucleo-h723z board to get started.I would like to have a ping example up and running, but I have not succeeded...I am using CUBEIDE V. 1.15.1 and CUBEMX V. 6.11.1.I have c...

DavidWahlberg_0-1716890710911.png DavidWahlberg_1-1716890788039.png DavidWahlberg_2-1716890822375.png DavidWahlberg_3-1716890840980.png

Webserver using AT Command

I'm having trouble using STM32 to bind to the Webserver via the AT Command command. Connecting to the Webserver is fine, but the problem is that the site only runs a few times, the AT+CIPSEND command has a problem, data sent to ESP is 1 character err...

dnk_0-1703649881431.png dnk_1-1703649907381.png dnk_2-1703649927893.png dnk_3-1703650046820.png
dnk by Associate
  • 2524 Views
  • 3 replies
  • 2 kudos

Resolved! In FreeRTOS, priority settings

Hello everyone,I am using FreeRTOS but i am confuse about seting priority, Should I give same priority to every task or different priority to all task.And also what is different between them.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.