STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Porting STM32F1 Firmware to STM32F4

Hey all, I want to port this https://github.com/ArduCAM/STM32/tree/master/STM32F103 package to use for an STM32F446RE development board. Can anyone offer any advice as to the best practices of accomplishing this? Would it be modifying mapping of GPIO...

CubeIDE and classB setup

We will be submitting our STM32F101vft based appliance for UL certification.  We found the self-test extension X-CUBE-CLASSB.   I review app note AN4435, and also found this community post from Christophe Vrignaud helpful. The example project STM3210...

HunterR by Associate II
  • 1104 Views
  • 0 replies
  • 0 kudos

Resolved! STM32_USB_Device_Library cannot be compiled

Helloi have problem to compile STM32Cube_FW_F7_V1.17.0\Middlewares\ST\STM32_USB_Device_LibraryI use STM32CubeIDE Version: 1.14.0 + STM32CubeMX Version: 6.10.0-RC9chip STM32F767ZITx  (NUCLEO-F767ZI)I'm mainly interested in the causeexpected '=', ',', ...

stm_err.png stm_err_2.png
PNova.2 by Associate II
  • 2763 Views
  • 3 replies
  • 1 kudos

Resolved! STM32 read from flash breaks freertos.

Hi,  This is a weird one. When my controller starts up, it is supposed to read the flash and use this data to check if my lwip should start up in DHCP mode or with a static IP adres.When I don't read from flash, this code works fine, when I do read f...

WilliamVR_2-1718106796722.png WilliamVR_1-1718106658676.png WilliamVR_0-1718106598884.png
WilliamVR by Associate III
  • 2038 Views
  • 1 replies
  • 0 kudos

Resolved! Problem with dynamicaly changing USB-C PDOs

Hello,I am trying to make my own custom USB PD application on NucleoG0B1RE + SNK1M1 hardware.I want to change dynamically the SNK PDOs in my application (it should be possible according to this post). Since I want it to be working with various Source...

Marosh by Associate III
  • 4348 Views
  • 6 replies
  • 6 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.