STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo STM32H743ZI Lan Interface does not work

Hello experts, what am I doing wrong? For days I have been trying to put the LAN interface of my STM32H743ZI board into operation. I just want to send a text to my PC and also be able to receive text from the PC. The board should be the server. Unfor...

0693W0000059NWcQAM.jpg 0693W0000059NWhQAM.jpg 0693W0000059NWmQAM.jpg 0693W0000059NWNQA2.jpg
HGumb.1 by Associate II
  • 2773 Views
  • 3 replies
  • 0 kudos

Custom Bootloader implementation on STM32L4S5

Hi,We are working on product based on STM32L4S5 based MCU. We implemented the bootloader which are able to boot from base address (binary image starting from base address 0x08022000). Current implementation doesn't have any validation.But due to secu...

usha by Associate
  • 2106 Views
  • 3 replies
  • 0 kudos

Resolved! RTC start time of the init mode

Hello,I've a project with the STM32G030F6 which use the RTC (SYSCLK=64MHz RTCCLK=32768Hz). During the setting of new date/time I enable the INIT mode with: LL_RTC_EnableInitMode (RTC); while (0u == READ_BIT (RTC->ICSR, RTC_ICSR_INITF)) { } The runtim...

bm2 by Associate III
  • 3600 Views
  • 6 replies
  • 0 kudos

HOW to reset nucleo H755 (blocked board)

Hola a todos, soy nuevo en STM32.Mi placa está bloqueada en este estado (ver en la foto): 2 LED en estado rojo continuamente. Busque en Google y descargue una copia de STM32 Cube Programmer, evita las tonterías de IDE/GDBRevisar el manual de la placa...

Imagen de WhatsApp 2024-06-13 a las 14.38.28_7aedc905.jpg
Fablax by Associate
  • 1389 Views
  • 2 replies
  • 0 kudos

High speed data transfer from STM32 to the PC

What is the best way to transfer high-speed data (12.288 Mbit/s) from the STM32H723 microcontroller to a PC? I'm controlling a four-channel audio codec (AK4619vn) and need to sample the FFT of the signal received from the ADC on the PC. The STM32 MCU...

Yusuf2 by Associate II
  • 3692 Views
  • 4 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.