STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Ethernet on stm32f767 For Dummies

Hi,I have a background in electrical engineering but am a complete beginner with embedded engineering. I've bought two nucleo f767zi boards with the goal to send information between them using Ethernet with the built in rj45 port. My goal right now i...

Resolved! ethernetif.c File and misra-c:2012 2.3 Issue(?)

In the ethernetif.c file,typedef enum{RX_ALLOC_OK = 0x00,RX_ALLOC_ERROR = 0x01} RxAllocStatusTypeDef; // Here, RxAllocStatusTypeDef type is not used.It says that RxAllocStatusTypeDef is not used, which violates misra-c:2012 2.3.Inferentially, this wo...

lovewar by Associate
  • 1228 Views
  • 1 replies
  • 0 kudos

Jump to bootloader from Azure RTOS

Hello,I'm having some issue going from my user code running azure RTOS to the bootloader. I'm using a STM32U599The code I'm using is the following, you can find online: void JumpToBootloader(void){uint32_t i=0;void (*SysMemBootJump)(void);/* Disable ...

STarlink by Associate
  • 1330 Views
  • 1 replies
  • 1 kudos

SMBUS STACK_SMBUS_ExecuteCommand on device

Hello everyoneI do not understand how to use the STACK_SMBUS_ExecuteCommand callback function provided by the SMBUS stack (See picture below). The function is called either in receiving data or transmitting data (from the device point of view). Due t...

image.png
VORDO by Associate
  • 1391 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.