STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Where to read length of sleep time on RTC WUT

We are using the STM32L071RB, currently have the firmware set to go to sleep (stop mode) and wake up after ~5 minutes with the RTC WUT (see section 22.4.6 and A13.3 in RM0377). This works great, however this timer isn't the only wakeup source. If the...

LWill.4 by Associate II
  • 3707 Views
  • 6 replies
  • 2 kudos

Resolved! HAL issue with int8_t instead of uint8_t

Hello ! I've been working on with LIS3MDL a magnetometer from STM, but there was one problem because reading X,Y,Z it was showing good values but sometimes instead of value it just spitted 0, for example X = 0.14, Y = 0.30, Z = 0.14 and sometimes it ...

Xenon02 by Senior
  • 6154 Views
  • 8 replies
  • 2 kudos

Resolved! STM32F4 UART NOT WORKING CORRECTLY

In the code I have written here, I am trying to send data from UART4 within the main function and simultaneously receive data through interrupts if data arrives. However, the data transmission part works for a very short time and then stops, and the ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.