2024-07-20 3:10 AM
Hello
I am working on the Free RTOS code that I am trying to send the data on the server using Free RTOS but I am not able to send data on the server I am using some dummy data and GPS for location +STM32F411ceu6a+EC200U GNSS. But my RTOS task is not working can some one plz help me find the problem in my code.
CODE:-
// Globals
QueueHandle_t xQueue;
SemaphoreHandle_t xBinarySemaphore;
typedef struct {
float Latitude;
float Longitude;
float objectTemp;
float ambientTemp;
float xG;
float yG;
float zG;
float avg;
} GPSData_t;
/* Definitions for ec200u6 */
osThreadId_t ec200u6Handle;
const osThreadAttr_t ec200u6_attributes = {
.name = "ec200u6",
.stack_size = 128* 4,
.priority = (osPriority_t) osPriorityRealtime,
};
/* Definitions for L89 */
osThreadId_t L89Handle;
const osThreadAttr_t L89_attributes = {
.name = "L89",
.stack_size = 128 * 4,
.priority = (osPriority_t) osPriorityRealtime,
};
/* Definitions for myQueue01 */
osMessageQueueId_t myQueue01Handle;
const osMessageQueueAttr_t myQueue01_attributes = {
.name = "myQueue01"
};
/* Definitions for myMutex01 */
osMutexId_t myMutex01Handle;
const osMutexAttr_t myMutex01_attributes = {
.name = "myMutex01"
};
/* Definitions for myBinarySem01 */
osSemaphoreId_t myBinarySem01Handle;
const osSemaphoreAttr_t myBinarySem01_attributes = {
.name = "myBinarySem01"
};
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
static void MX_ADC1_Init(void);
static void MX_I2C1_Init(void);
static void MX_SPI1_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_USART6_UART_Init(void);
void Startec200u6(void *argument);
void StartL89(void *argument);
// Create the queue
xQueue = xQueueCreate(10, sizeof(GPSData_t)); // Adjust the size as needed
// Create the binary semaphore
xBinarySemaphore = xSemaphoreCreateBinary();
if (xQueue != NULL && xBinarySemaphore != NULL)
{
// Create the tasks
xTaskCreate(Startec200u6, "Task2", configMINIMAL_STACK_SIZE, NULL, 1, NULL);
xTaskCreate(StartL89, "Task1", configMINIMAL_STACK_SIZE, NULL, 1, NULL);
// Start the scheduler
vTaskStartScheduler();
}
/* USER CODE END 2 */
/* Init scheduler */
osKernelInitialize();
/* Create the mutex(es) */
/* creation of myMutex01 */
myMutex01Handle = osMutexNew(&myMutex01_attributes);
/* USER CODE BEGIN RTOS_MUTEX */
/* add mutexes, ... */
/* USER CODE END RTOS_MUTEX */
/* Create the semaphores(s) */
/* creation of myBinarySem01 */
myBinarySem01Handle = osSemaphoreNew(1, 1, &myBinarySem01_attributes);
/* USER CODE BEGIN RTOS_SEMAPHORES */
/* add semaphores, ... */
/* USER CODE END RTOS_SEMAPHORES */
/* USER CODE BEGIN RTOS_TIMERS */
/* start timers, add new ones, ... */
/* USER CODE END RTOS_TIMERS */
/* Create the queue(s) */
/* creation of myQueue01 */
myQueue01Handle = osMessageQueueNew (16, sizeof(uint16_t), &myQueue01_attributes);
/* USER CODE BEGIN RTOS_QUEUES */
/* add queues, ... */
/* USER CODE END RTOS_QUEUES */
/* Create the thread(s) */
/* creation of ec200u6 */
ec200u6Handle = osThreadNew(Startec200u6, NULL, &ec200u6_attributes);
/* creation of L89 */
L89Handle = osThreadNew(StartL89, NULL, &L89_attributes);
/* USER CODE BEGIN RTOS_THREADS */
/* add threads, ... */
/* USER CODE END RTOS_THREADS */
/* USER CODE BEGIN RTOS_EVENTS */
/* add events, ... */
/* USER CODE END RTOS_EVENTS */
vTaskStartScheduler();
/* Start scheduler */
// osKernelStart();
void Startec200u6(void *pvParameters)
{
/* USER CODE BEGIN 5 */
/* Infinite loop */
GPSData_t receivedData;
int retryCount;
const int maxRetries = 2;
for (;;) // Infinite loop for the task
{
if (xSemaphoreTake(xBinarySemaphore, portMAX_DELAY) == pdTRUE)
{
if (xQueueReceive(xQueue, &receivedData, portMAX_DELAY) == pdPASS)
{
// Retry sending data up to maxRetries times
retryCount = 0;
while (!sendHTTP(receivedData.Latitude, receivedData.Longitude,
receivedData.objectTemp, receivedData.ambientTemp,
receivedData.xG, receivedData.yG, receivedData.zG,
receivedData.avg))
{
vTaskDelay(pdMS_TO_TICKS(2000)); // Delay for 2000 ms
if (retryCount < maxRetries)
{
retryCount++;
}
else
{
break;
}
}
}
}
}
/* USER CODE END 5 */
}
void StartL89(void *pvParameters)
{
/* USER CODE BEGIN StartL89 */
GPSData_t gpsData;
for (;;) // Infinite loop for the task
{
// Receive data from UART
HAL_UART_Receive(&huart2, (uint8_t *)Rxdata, 700, 5000);
// Get location data
get_location(&gpsData.Latitude, &gpsData.Longitude, 0);
// Populate other sensor data
gpsData.objectTemp = 25.0; // Predefined value for object temperature
gpsData.ambientTemp = 24.0; // Predefined value for ambient temperature
gpsData.xG = 0.1; // Predefined value for X-axis acceleration
gpsData.yG = 0.2; // Predefined value for Y-axis acceleration
gpsData.zG = 0.3; // Predefined value for Z-axis acceleration
gpsData.avg = (gpsData.xG + gpsData.yG + gpsData.zG) / 3.0; // Calculate average
// Toggle the pin to indicate data reception
L89_TogglePin(2, 3);
// Attempt to send the data to the queue
if (xQueueSend(xQueue, &gpsData, portMAX_DELAY) != pdPASS)
{
// Handle queue send error
}
else
{
// Data was successfully queued, give the semaphore
xSemaphoreGive(xBinarySemaphore);
}
}
/* USER CODE END StartL89 */
}
2024-07-20 12:18 PM
Have you tried some advices from this thread?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.