STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADC Sampling and Display

As is well known, the ADC sampling rate is on the order of microseconds, while the display task may only refresh once every 100 milliseconds. In an RTOS, how can the display task and ADC sampling values be synchronized? With such a long display refre...

xwq370 by Associate
  • 272 Views
  • 2 replies
  • 1 kudos

Resolved! X-CUBE-GNSS1

I have a project that will be using the LIV4F chip. I downloaded and installed X-CUBE-GNSS1 but its description says it is for the LIV3F. Is it compatible with and will it function with the LIV4F chip? I will be using it on the STM32G474CEU6.Thanks!

hritter by Associate II
  • 224 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H533 and CubeMX generated project for CubeIDE

Hello, all my tools are updated to last ones, and software packages too. I start an empty project using X Cube FreeRtos 1.5 (just a default task). Play the soft with debug, and after a few seconds, press "Suspend" button to break the running program....

lclor by Associate III
  • 1478 Views
  • 16 replies
  • 0 kudos

STM32H5 - I3C access to IKS4A1

Hello Folks, sorry, I am quite desperate. I try to get my I3C code working, but the read consistently fails and returns a buffer with just 255s and a temperature of 350 degrees centigrade.   The weird thing is that the checks I put in work, so it loo...

THANN.1 by Associate II
  • 275 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.